Common Name: GRINDING AND CUTTING WHEELS, RESINOID (TYPE 1, TYPE 27, TYPE 28, TYPE 29), CUP W
Manufacturer: UNITED ABRASIVES
SDS Revision Date: 9/22/2015
SDS Format: ANSI-OSHA
   
Grainger Item Number(s): 5LUC1
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. PRODUCT AND COMPANY IDENTIFICATION 
2. HAZARDS IDENTIFICATION 
3. COMPOSITION/INFORMATION ON INGREDIENTS 
4. FIRST AID MEASURES 
5. FIRE FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS/PERSONAL PROTECTION 
9. PHYSICAL AND CHEMICAL PROPERTIES 
10. STABILITY AND REACTIVITY 
11. TOXICOLOGICAL INFORMATION 
12. ECOLOGICAL INFORMATION 
13. DISPOSAL CONSIDERATIONS 
14. TRANSPORT INFORMATION 
15. REGULATORY INFORMATION 
16. OTHER INFORMATION 



UA
UNITED ABRASIVES, INC.

MATERIAL SAFETY DATA SHEET

RESINOID BONDED ABRASIVES

MSDS: # 1/2


1. PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT IDENTITY / TRADE NAME:
GRINDING AND CUTTING WHEELS, RESINOID (TYPE 1, TYPE 27, TYPE 28, TYPE 29),
CUP WHEELS (TYPE 11) CONES AND PLUGS (TYPE 16, TYPE 17 AND TYPE 18),
MOUNTED POINTS

PRODUCT USE:
ABRASIVE MATERIALS USED FOR CUTTING AND GRINDING METALS, CONCRETE, MASONRY
AND BUILDING MATERIALS.

MANUFACTURER:
UNITED ABRASIVES, INC.
185 BOSTON POST ROAD
NORTH WINDHAM, CT 06256

INTERNET: WWW.UNITEDABRASIVES.COM

INFORMATION PHONE: (860) 456-7131

EMERGENCY PHONE: (860) 456-7131

MSDS DATE OF PREPARATION: SEPTEMBER 22, 2015


2. HAZARDS IDENTIFICATION 


THIS PRODUCT IS A BLACK, BROWN OR REDDISH COLORED SOLID WHEEL WITH NO ODOR.

EMERGENCY OVERVIEW:
DUST MAY CAUSE EYE AND RESPIRATORY IRRITATION. DUST PARTICLES MAY CAUSE
ABRASIVE INJURY TO THE EYES.


3. COMPOSITION/INFORMATION ON INGREDIENTS 


HAZARDOUS COMPONENT                        CAS #            %

ALUMINUM OXIDE                              1344-28-1       0-95

SILICON CARBIDE                              409-21-2       0-95

ZIRCONIUM OXIDE                             1314-23-4       0-80

CURED PHENOLIC RESIN                       N/A              1-30

NITRILE COMPOUNDS                          N/A              1-20

FLUORIDE COMPOUNDS                         N/A              1-20

IRON PYRITE                                12068-85-8       0-20

WOVEN FIBERGLASS                           N/A              0-15

CALCIUM COMPOUNDS                          N/A              0-15

SULFUR                                      7704-34-9       0-15

CALCIUM OXIDE                               1305-78-8       1-10

CRYOLITE                                   15096-52-3       1-10

CURED EPOXY RESIN                          N/A              1-10

TITANIUM DIOXIDE                           13463-67-7       0-5

CALCIUM CARBONATE                           1317-65-3       0-5

ALUMINUM POTASSIUM FLUORIDE                14484-69-6       0-5

IRON OXIDE                                  1309-37-1       0-5

GRAPHITE                                    7782-42-5       0-5

POTASSIUM FLUOROBORATE                     14075-53-7       0-5


4. FIRST AID MEASURES 


INGESTION: IF GRINDING DUST IS SWALLOWED, SEEK MEDICAL ATTENTION.

INHALATION:
IF OVEREXPOSED TO GRINDING DUST, REMOVE VICTIM TO FRESH AIR AND GET MEDICAL
ATTENTION.

EYE CONTACT:
FLUSH EYES THOROUGHLY WITH WATER, HOLDING OPEN EYELIDS. GET MEDICAL
ATTENTION IF IRRITATION PERSISTS. OBTAIN IMMEDIATE MEDICAL ATTENTION FOR
FOREIGN BODY IN THE EYE.

SKIN CONTACT:
WASH DUST FROM SKIN WITH SOAP AND WATER. LAUNDER CONTAMINATED CLOTHING
BEFORE REUSE.


5. FIRE FIGHTING MEASURES 


EXTINGUISHING MEDIA:
USE ANY MEDIA THAT IS APPROPRIATE FOR THE SURROUNDING FIRE.

SPECIAL FIREFIGHTING PROCEDURES: NONE NEEDED.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
THIS PRODUCT IS NOT COMBUSTIBLE, HOWEVER, CONSIDERATION MUST BE GIVEN TO
THE POTENTIAL FIRE/EXPLOSION HAZARDS FROM THE BASE MATERIAL BEING
PROCESSED. MANY MATERIALS CREATE FLAMMABLE/EXPLOSIVE DUSTS OR TURNINGS
WHEN MACHINED OR GROUND.

HAZARDOUS COMBUSTION PRODUCTS: NONE KNOWN.


6. ACCIDENTAL RELEASE MEASURES 


PICK UP, SWEEP UP OR VACUUM AND PLACE IN A CONTAINER FOR DISPOSAL. MINIMIZE
GENERATION OF DUST. NOTIFY AUTHORITIES AS REQUIRED BY LOCAL, STATE AND
FEDERAL REGULATIONS.


7. HANDLING AND STORAGE 


RECOMMENDED WORK PRACTICES:
USE ONLY WITH ADEQUATE VENTILATION. AVOID BREATHING DUST. WASH THOROUGHLY
AFTER HANDLING AND USE, ESPECIALLY BEFORE EATING, DRINKING OR SMOKING.
REFER TO ANSI B7.1, SAFETY REQUIREMENTS FOR THE USE, CARE AND PROTECTION OF
ABRASIVE WHEELS FOR ADDITIONAL INFORMATION. CONSIDER POTENTIAL EXPOSURE TO
COMPONENTS OF THE BASE MATERIALS OR COATINGS BEING GROUND. REFER TO OSHA'S
SUBSTANCE SPECIFIC STANDARDS FOR ADDITIONAL WORK PRACTICE REQUIREMENTS
WHERE APPLICABLE.

STORAGE:
STORE IN ACCORDANCE WITH ANSI B7.1. PROTECT ABRASIVE WHEELS FROM DAMAGE.


8. EXPOSURE CONTROLS/PERSONAL PROTECTION 


EXPOSURE GUIDELINES:

HAZARDOUS COMPONENT            OSHA PEL            ACGIH TLV

ALUMINUM OXIDE                 5 MG/M3             1 MG/M3 (RESPIRABLE)
                               (RESPIRABLE         (AS Al METAL)
                               FRACTION)

                               15 MG/M3
                               (TOTAL DUST)

SILICON CARBIDE                NONE ESTABLISHED    10 MG/M3 (INHALABLE)
                                                   3 MG/M3 (RESPIRABLE)

ZIRCONIUM OXIDE                5 MG/M3             5 MG/M3
(AS ZIRCOMIUM COMPOUNDS)                           10 MG/M3 STEL

CURED PHENOLIC RESIN           NONE ESTABLISHED    NONE ESTABLISHED

NITRILE COMPOUNDS              NONE ESTABLISHED    NONE ESTABLISHED

FLUORIDE COMPOUNDS             2.5 MG/M3           2.5 MG/M3

IRON PYRITE                    NONE ESTABLISHED    NONE ESTABLISHED

WOVEN FIBERGLASS               5 MG/M3             5 MG/M3 (INHALABLE)
                               (RESPIRABLE         1 F/CC
                               FRACTION)

                               15 MG/M3
                               (TOTAL DUST)

CALCIUM COMPOUNDS              NONE ESTABLISHED    NONE ESTABLISHED

SULFUR                         NONE ESTABLISHED    NONE ESTABLISHED

CALCIUM OXIDE                  5 MG/M3             2 MG/M3

CRYOLITE (AS FLUORIDES)        2.5 MG/M3           2.5 MG/M3

CURED EPOXY RESIN              NONE ESTABLISHED    NONE ESTABLISHED

TITANIUM DIOXIDE               15 MG/M3            10 MG/M3
                               (TOTAL DUST)

CALCIUM CARBONATE              5 MG/M3             NONE ESTABLISHED
                               (RESPIRABLE
                               FRACTION)

                               15 MG/M3
                               (TOTAL DUST)

ALUMINUM POTASSIUM FLUORIDE    5 MG/M3             1 MG/M3 (RESPIRABLE)
(AS Al METAL                   (RESPIRABLE
                               FRACTION)

                               15 MG/M3
                               (TOTAL DUST)

ALUMINUM POTASSIUM FLUORIDE    2.5 MG/M3           2.5 MG/M3
(AS FLUORIDES)

IRON OXIDE                     10 MG/M3 (FUME)     5 MG/M3 (RESPIRABLE)

GRAPHITE                       15 MPPCF            2 MG/M3 (RESPIRABLE)

POTASSIUM FLUOROBORATE         2.5 MG/M3           2.5 MG/M3
(AS FLUORIDES)

NOTE: CONSIDER ALSO COMPONENTS OF BASE MATERIALS AND COATINGS BEING GROUND.

VENTILATION:
USE LOCAL EXHAUST OR GENERAL VENTILATION AS REQUIRED TO MINIMIZE EXPOSURE
TO DUST AND MAINTAIN THE CONCENTRATION OF CONTAMINANTS BELOW THE TLVS.

RESPIRATORY PROTECTION:
USE NIOSH APPROVED RESPIRATOR IF EXPOSURE LIMITS ARE EXCEEDED OR WHERE DUST
EXPOSURES ARE EXCESSIVE. CONSIDER THE POTENTIAL FOR EXPOSURE TO COMPONENTS
OF THE COATINGS OR BASE MATERIAL BEING GROUND IN SELECTING PROPER
RESPIRATORY PROTECTION. REFER TO OSHA'S SPECIFIC STANDARDS FOR LEAD,
CADMIUM, ETC. WHERE APPROPRIATE. SELECTION OF RESPIRATORY PROTECTION
DEPENDS ON THE CONTAMINANT TYPE, FORM AND CONCENTRATION. SELECT AND USE
RESPIRATORS IN ACCORDANCE WITH OSHA 1910.134 AND GOOD INDUSTRIAL HYGIENE
PRACTICE.

GLOVES: CLOTH OR LEATHER GLOVES RECOMMENDED.

EYE PROTECTION:
SAFETY GOGGLES OR FACE SHIELD OVER SAFETY GLASSES WITH SIDE SHIELDS.

OTHER:
PROTECTIVE CLOTHING AS NEEDED TO PREVENT CONTAMINATION OF PERSONAL
CLOTHING. HEARING PROTECTION MAY BE REQUIRED.


9. PHYSICAL AND CHEMICAL PROPERTIES 


BOILING POINT: NOT APPLICABLE

VAPOR PRESSURE (MMHg): NOT APPLICABLE

SOLUBILITY IN WATER: INSOLUBLE

VAPOR DENSITY (AIR = 1): NOT APPLICABLE

SPECIFIC GRAVITY: NOT APPLICABLE

EVAPORATION RATE: NOT APPLICABLE

MELTING POINT: NOT APPLICABLE

FLASH POINT: NON-COMBUSTIBLE

FLAMMABLE LIMITS:
LEL: NOT APPLICABLE
UEL: NOT APPLICABLE

APPEARANCE AND ODOR:
BLACK, BROWN OR REDDISH COLORED SOLID WHEEL WITH NO ODOR.


10. STABILITY AND REACTIVITY 


STABILITY: STABLE

INCOMPATIBILITY: NONE KNOWN.

HAZARDOUS DECOMPOSITION PRODUCTS:
DUST FROM GRINDING COULD CONTAIN INGREDIENTS LISTED IN SECTION 3 AND OTHER,
POTENTIALLY MORE HAZARDOUS COMPONENTS OF THE BASE MATERIAL BEING GROUND OR
COATINGS APPLIED TO THE BASE MATERIAL.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.


11. TOXICOLOGICAL INFORMATION 


HEALTH HAZARDS:

INGESTION:
NONE EXPECTED UNDER NORMAL USE CONDITIONS. SWALLOWING LARGE PIECES MAY
CAUSE OBSTRUCTION OF THE GASTROINTESTINAL TRACT.

INHALATION: DUST MAY CAUSE RESPIRATORY IRRITATION.

EYE:
DUST MAY CAUSE EYE IRRITATION. DUST PARTICLES MAY CAUSE ABRASIVE INJURY TO
THE EYES.

SKIN:
NONE EXPECTED UNDER NORMAL USE CONDITIONS. RUBBING PRODUCT ACROSS THE SKIN
MAY CAUSE MECHANICAL IRRITATION OR ABRASIONS.

SENSITIZATION: THIS MATERIAL IS NOT KNOWN TO CAUSE SENSITIZATION.

CHRONIC:
LONG-TERM OVEREXPOSURE TO RESPIRABLE DUST MAY CAUSE LUNG DAMAGE (FIBROSIS)
WITH SYMPTOMS OF COUGHING, SHORTNESS OF BREATH AND DIMINISHED BREATHING
CAPACITY. CHRONIC EFFECTS MAY BE AGGRAVATED BY SMOKING. PROLONGED
OVEREXPOSURE TO FLUORIDES MAY CAUSE A BONE CONDITION, FLUOROSIS. PROLONGED
EXPOSURE TO ELEVATED NOISE LEVELS DURING OPERATIONS MAY AFFECT HEARING. A
GREATER HAZARD, IN MOST CASES, IS THE EXPOSURE TO THE DUST/FUMES FROM THE
MATERIAL OR PAINT/COATINGS BEING GROUND. MOST OF THE DUST GENERATED DURING
GRINDING IS FROM THE BASE MATERIAL BEING GROUND AND THE POTENTIAL HAZARD
FROM THIS EXPOSURE MUST BE EVALUATED.

CARCINOGENICITY:
TITANIUM DIOXIDE IS LISTED BY IARC AS A GROUP 2B CARCINOGEN (SUSPECTED
HUMAN CARCINOGEN). NONE OF THE OTHER COMPONENTS IS LISTED AS A CARCINOGEN
OR POTENTIAL CARCINOGEN BY OSHA, NTP OR IARC.

MEDICAL CONDITIONS AGGRAVATED BY EXPOSURE:
EMPLOYEES WITH PRE-EXISTING RESPIRATORY DISEASE MAY BE AT RISK FROM
EXPOSURE.

ACUTE TOXICITY VALUES:
THIS PRODUCT AND ITS COMPONENTS ARE NOT ACUTELY TOXIC. THE ONLY ACUTE
TOXICITY DATA AVAILABLE FOR THE COMPONENTS ARE LISTED BELOW.

ALUMINUM OXIDE:
ORAL RAT LD50: >5,000 MG/KG

CRYOLITE:
ORAL RAT LD50: >5,000 MG/KG


12. ECOLOGICAL INFORMATION 


NO ECOLOGICAL DATA IS AVAILABLE FOR THIS PRODUCT. NO HAZARDS TO THE
ENVIRONMENT ARE EXPECTED FROM THIS PRODUCT. HOWEVER, CONSIDERATION MUST
BE GIVEN TO POTENTIAL ENVIRONMENT EFFECTS OF THE BASE MATERIAL BEING
PROCESSED.


13. DISPOSAL CONSIDERATIONS 


DISPOSE IN ACCORDANCE WITH ALL APPLICABLE LOCAL, STATE/PROVINCIAL AND
FEDERAL REGULATIONS. LOCAL REGULATIONS MAY BE MORE STRINGENT THAN REGIONAL
AND NATIONAL REQUIREMENTS. IT IS THE RESPONSIBILITY OF THE WASTE GENERATOR
TO DETERMINE THE TOXICITY AND PHYSICAL CHARACTERISTICS OF THE MATERIAL TO
DETERMINE THE PROPER WASTE IDENTIFICATION AND DISPOSAL IN COMPLIANCE WITH
APPLICABLE REGULATIONS.


14. TRANSPORT INFORMATION 


DOT HAZARDOUS MATERIALS DESCRIPTION:

PROPER SHIPPING NAME: NOT REGULATED

UN NUMBER: NONE

HAZARD CLASS/PACKING GROUP: NONE

LABELS REQUIRED: NONE


15. REGULATORY INFORMATION 


SARA SECTION 311/312 HAZARD CATEGORIES:
NOT APPLICABLE (MANUFACTURED ARTICLES)

SARA SECTION 313:
SOME PRODUCTS CONTAIN THE FOLLOWING TOXIC CHEMICALS SUBJECT TO THE
REPORTING REQUIREMENTS OF SECTION 313 OF TITLE III OF THE SUPERFUND
AMENDMENTS AND REAUTHORIZATION ACT OF 1986 AND 40 CFR PART 372
(TOXIC CHEMICAL RELEASE REPORTING): NONE

CALIFORNIA PROPOSITION 65:

WARNING:
YOU CREATE DUST WHEN YOU CUT, SAND, DRILL OR GRIND MATERIALS SUCH AS WOOD,
PAINT, CEMENT, MASONRY OR METAL. THIS DUST OFTEN CONTAINS CHEMICALS KNOWN
TO CAUSE CANCER, BIRTH DEFECTS OR OTHER REPRODUCTIVE HARM.

CANADIAN WHMIS CLASSIFICATION:
NOT A CONTROLLED PRODUCT. THIS PRODUCT MEETS THE DEFINITION OF A
"MANUFACTURED ARTICLE" UNDER THE WHMIS REGULATIONS.

THIS PRODUCT HAS BEEN CLASSIFIED UNDER THE CPR AND THIS MSDS DISCLOSES
INFORMATION ELEMENTS REQUIRED BY THE CPR.


16. OTHER INFORMATION 


NFPA HAZARD RATING:
HEALTH     1
FIRE       0
REACTIVITY 0

DATE PREVIOUS REVISION: 12/1/09

DATE THIS REVISION: 9/22/15

REVISION SUMMARY:
SECTION 3 UPDATED COMPOSITION, SECTION 8 UPDATED EXPOSURE LIMITS,
SECTION 11 UPDATED ACUTE TOXICITY VALUES.

THE PRECEDING INFORMATION IS BELIEVED TO BE CORRECT AND CURRENT AS OF THE
DATE OF PREPARATION OF THIS MATERIAL SAFETY DATA SHEET. SINCE THE USE OF
THIS INFORMATION AND THE CONDITIONS OF USE OF THIS PRODUCT ARE NOT WITHIN
THE CONTROL OF UNITED ABRASIVES, INC., IT IS THE USER'S OBLIGATION TO
ASSURE SAFE USE OF THIS PRODUCT.