Common Name: CD 887 COIL & FIN CLEANER AEROSOL
Manufacturer: SPRAYON PRODUCTS
SDS Revision Date: 5/22/2015
SDS Format: GHS-US
   
Grainger Item Number(s): 1MEU7
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1. IDENTIFICATION 
SECTION 2. HAZARDS IDENTIFICATION 
SECTION 3. COMPOSITION/INFORMATION ON INGREDIENTS 
SECTION 4. FIRST AID MEASURES 
SECTION 5. FIRE-FIGHTING MEASURES 
SECTION 6. ACCIDENTAL RELEASE MEASURES 
SECTION 7. HANDLING AND STORAGE 
SECTION 8. EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10. STABILITY AND REACTIVITY 
SECTION 11. TOXICOLOGICAL INFORMATION 
SECTION 12. ECOLOGICAL INFORMATION 
SECTION 13. DISPOSAL CONSIDERATIONS 
SECTION 14. TRANSPORT INFORMATION 
SECTION 15. REGULATORY INFORMATION 
SECTION 16. OTHER INFORMATION 



SAFETY DATA SHEET

S00887000


SECTION 1. IDENTIFICATION 


PRODUCT NAME: CD(TM)887 COIL & FIN CLEANER AEROSOL

PRODUCT CODE: S00887000

OTHER MEANS OF IDENTIFICATION: NOT AVAILABLE.

PRODUCT TYPE: AEROSOL.

RELEVANT IDENTIFIED USES OF THE SUBSTANCE OR MIXTURE AND USES ADVISED
AGAINST: NOT APPLICABLE.

MANUFACTURER:
SPRAYON PRODUCTS
CLEVELAND, OH 44115

EMERGENCY TELEPHONE NUMBER OF THE COMPANY: (216) 566-2917

PRODUCT INFORMATION TELEPHONE NUMBER: (800)247-3266

REGULATORY INFORMATION TELEPHONE NUMBER: (216)566-2902

TRANSPORTATION EMERGENCY TELEPHONE NUMBER: (800)424-9300


SECTION 2. HAZARDS IDENTIFICATION 


OSHA/HCS STATUS:
THIS MATERIAL IS CONSIDERED HAZARDOUS BY THE OSHA HAZARD COMMUNICATION
STANDARD (29 CFR 1910.1200).

CLASSIFICATION OF THE SUBSTANCE OR MIXTURE:
FLAMMABLE AEROSOLS: CATEGORY 1

GASES UNDER PRESSURE: COMPRESSED GAS

SKIN CORROSION/IRRITATION: CATEGORY 1

SERIOUS EYE DAMAGE/EYE IRRITATION: CATEGORY 1

SPECIFIC TARGET ORGAN TOXICITY (REPEATED EXPOSURE): CATEGORY 2

PERCENTAGE OF THE MIXTURE CONSISTING OF INGREDIENT(S) OF UNKNOWN TOXICITY:
1.6%

GHS LABEL ELEMENTS:

HAZARD PICTOGRAMS:
FLAME
GAS CYLINDER
CORROSION
HEALTH HAZARD

SIGNAL WORD: DANGER

HAZARD STATEMENTS:
EXTREMELY FLAMMABLE AEROSOL.
CONTAINS GAS UNDER PRESSURE; MAY EXPLODE IF HEATED.
CAUSES SEVERE SKIN BURNS AND EYE DAMAGE.
MAY CAUSE DAMAGE TO ORGANS THROUGH PROLONGED OR REPEATED EXPOSURE.

PRECAUTIONARY STATEMENTS:

PREVENTION:
WEAR PROTECTIVE GLOVES. WEAR EYE OR FACE PROTECTION. WEAR PROTECTIVE
CLOTHING. KEEP AWAY FROM HEAT, HOT SURFACES, SPARKS, OPEN FLAMES AND OTHER
IGNITION SOURCES. NO SMOKING.

PRESSURIZED CONTAINER:
DO NOT PIERCE OR BURN, EVEN AFTER USE. DO NOT SPRAY ON AN OPEN FLAME OR
OTHER IGNITION SOURCE. DO NOT BREATHE DUST OR MIST. WASH HANDS THOROUGHLY
AFTER HANDLING.

RESPONSE: GET MEDICAL ATTENTION IF YOU FEEL UNWELL.

IF INHALED:
REMOVE VICTIM TO FRESH AIR AND KEEP AT REST IN A POSITION COMFORTABLE FOR
BREATHING. IMMEDIATELY CALL A POISON CENTER OR PHYSICIAN.

IF SWALLOWED:
IMMEDIATELY CALL A POISON CENTER OR PHYSICIAN. RINSE MOUTH. DO NOT INDUCE
VOMITING.

IF ON SKIN (OR HAIR):
TAKE OFF IMMEDIATELY ALL CONTAMINATED CLOTHING. RINSE SKIN WITH WATER OR
SHOWER. WASH CONTAMINATED CLOTHING BEFORE REUSE. IMMEDIATELY CALL A POISON
CENTER OR PHYSICIAN.

IF IN EYES:
RINSE CAUTIOUSLY WITH WATER FOR SEVERAL MINUTES. REMOVE CONTACT LENSES, IF
PRESENT AND EASY TO DO. CONTINUE RINSING. IMMEDIATELY CALL A POISON CENTER
OR PHYSICIAN.

STORAGE:
STORE LOCKED UP. PROTECT FROM SUNLIGHT. DO NOT EXPOSE TO TEMPERATURES
EXCEEDING 50 DEG. C/122 DEG. F. STORE IN A WELL-VENTILATED PLACE.

DISPOSAL:
DISPOSE OF CONTENTS AND CONTAINER IN ACCORDANCE WITH ALL LOCAL, REGIONAL,
NATIONAL AND INTERNATIONAL REGULATIONS.

SUPPLEMENTAL LABEL ELEMENTS:

WARNING:
THIS PRODUCT CONTAINS CHEMICALS KNOWN TO THE STATE OF CALIFORNIA TO CAUSE
CANCER AND BIRTH DEFECTS OR OTHER REPRODUCTIVE HARM. FOR INDUSTRIAL USE
ONLY.

PLEASE REFER TO THE SDS FOR ADDITIONAL INFORMATION. KEEP UPRIGHT IN A COOL,
DRY PLACE. DO NOT DISCARD EMPTY CAN IN TRASH COMPACTOR.

HAZARDS NOT OTHERWISE CLASSIFIED: NONE KNOWN.


SECTION 3. COMPOSITION/INFORMATION ON INGREDIENTS 


SUBSTANCE/MIXTURE: MIXTURE

OTHER MEANS OF IDENTIFICATION: NOT AVAILABLE.

CAS NUMBER/OTHER IDENTIFIERS:

INGREDIENT NAME                           % BY WEIGHT         CAS NUMBER

BUTANE                                    3.4                 106-97-8

2-BUTOXYETHANOL                           2.0                 111-76-2

2-(2-ETHOXYETHOXY)-ETHANOL                2.0                 111-90-0

PROPANE                                   1.6                  74-98-6

TETRASODIUM ETHYLENEDIAMINETETRAACETATE   1.6                  64-02-8

THERE ARE NO ADDITIONAL INGREDIENTS PRESENT WHICH, WITHIN THE CURRENT
KNOWLEDGE OF THE SUPPLIER AND IN THE CONCENTRATIONS APPLICABLE, ARE
CLASSIFIED AS HAZARDOUS TO HEALTH OR THE ENVIRONMENT AND HENCE REQUIRE
REPORTING IN THIS SECTION.

OCCUPATIONAL EXPOSURE LIMITS, IF AVAILABLE, ARE LISTED IN SECTION 8.


SECTION 4. FIRST AID MEASURES 


DESCRIPTION OF NECESSARY FIRST AID MEASURES:

EYE CONTACT:
GET MEDICAL ATTENTION IMMEDIATELY. CALL A POISON CENTER OR PHYSICIAN.
IMMEDIATELY FLUSH EYES WITH PLENTY OF WATER, OCCASIONALLY LIFTING THE
UPPER AND LOWER EYELIDS. CHECK FOR AND REMOVE ANY CONTACT LENSES. CONTINUE
TO RINSE FOR AT LEAST 10 MINUTES. CHEMICAL BURNS MUST BE TREATED PROMPTLY
BY A PHYSICIAN.

INHALATION:
GET MEDICAL ATTENTION IMMEDIATELY. CALL A POISON CENTER OR PHYSICIAN.
REMOVE VICTIM TO FRESH AIR AND KEEP AT REST IN A POSITION COMFORTABLE FOR
BREATHING. IF IT IS SUSPECTED THAT FUMES ARE STILL PRESENT, THE RESCUER
SHOULD WEAR AN APPROPRIATE MASK OR SELF-CONTAINED BREATHING APPARATUS. IF
NOT BREATHING, IF BREATHING IS IRREGULAR OR IF RESPIRATORY ARREST OCCURS,
PROVIDE ARTIFICIAL RESPIRATION OR OXYGEN BY TRAINED PERSONNEL. IT MAY BE
DANGEROUS TO THE PERSON PROVIDING AID TO GIVE MOUTH-TO-MOUTH RESUSCITATION.
IF UNCONSCIOUS, PLACE IN RECOVERY POSITION AND GET MEDICAL ATTENTION
IMMEDIATELY. MAINTAIN AN OPEN AIRWAY. LOOSEN TIGHT CLOTHING SUCH AS A
COLLAR, TIE, BELT OR WAISTBAND. IN CASE OF INHALATION OF DECOMPOSITION
PRODUCTS IN A FIRE, SYMPTOMS MAY BE DELAYED. THE EXPOSED PERSON MAY NEED TO
BE KEPT UNDER MEDICAL SURVEILLANCE FOR 48 HOURS.

SKIN CONTACT:
GET MEDICAL ATTENTION IMMEDIATELY. CALL A POISON CENTER OR PHYSICIAN. FLUSH
CONTAMINATED SKIN WITH PLENTY OF WATER. REMOVE CONTAMINATED CLOTHING AND
SHOES. WASH CONTAMINATED CLOTHING THOROUGHLY WITH WATER BEFORE REMOVING IT,
OR WEAR GLOVES. CONTINUE TO RINSE FOR AT LEAST 10 MINUTES. CHEMICAL BURNS
MUST BE TREATED PROMPTLY BY A PHYSICIAN. WASH CLOTHING BEFORE REUSE. CLEAN
SHOES THOROUGHLY BEFORE REUSE.

INGESTION:
GET MEDICAL ATTENTION IMMEDIATELY. CALL A POISON CENTER OR PHYSICIAN. WASH
OUT MOUTH WITH WATER. REMOVE DENTURES IF ANY. REMOVE VICTIM TO FRESH AIR
AND KEEP AT REST IN A POSITION COMFORTABLE FOR BREATHING. IF MATERIAL HAS
BEEN SWALLOWED AND THE EXPOSED PERSON IS CONSCIOUS, GIVE SMALL QUANTITIES
OF WATER TO DRINK. STOP IF THE EXPOSED PERSON FEELS SICK AS VOMITING MAY BE
DANGEROUS. DO NOT INDUCE VOMITING UNLESS DIRECTED TO DO SO BY MEDICAL
PERSONNEL. IF VOMITING OCCURS, THE HEAD SHOULD BE KEPT LOW SO THAT VOMIT
DOES NOT ENTER THE LUNGS. CHEMICAL BURNS MUST BE TREATED PROMPTLY BY A
PHYSICIAN. NEVER GIVE ANYTHING BY MOUTH TO AN UNCONSCIOUS PERSON. IF
UNCONSCIOUS, PLACE IN RECOVERY POSITION AND GET MEDICAL ATTENTION
IMMEDIATELY. MAINTAIN AN OPEN AIRWAY. LOOSEN TIGHT CLOTHING SUCH AS A
COLLAR, TIE, BELT OR WAISTBAND.

MOST IMPORTANT SYMPTOMS/EFFECTS, ACUTE AND DELAYED:

POTENTIAL ACUTE HEALTH EFFECTS:

EYE CONTACT: CAUSES SERIOUS EYE DAMAGE.

INHALATION:
MAY GIVE OFF GAS, VAPOR OR DUST THAT IS VERY IRRITATING OR CORROSIVE TO THE
RESPIRATORY SYSTEM. EXPOSURE TO DECOMPOSITION PRODUCTS MAY CAUSE A HEALTH
HAZARD. SERIOUS EFFECTS MAY BE DELAYED FOLLOWING EXPOSURE.

SKIN CONTACT: CAUSES SEVERE BURNS.

INGESTION: MAY CAUSE BURNS TO MOUTH, THROAT AND STOMACH.

OVER-EXPOSURE SIGNS/SYMPTOMS:

EYE CONTACT:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
PAIN
WATERING
REDNESS

INHALATION:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
RESPIRATORY TRACT IRRITATION
COUGHING

SKIN CONTACT:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
PAIN OR IRRITATION
REDNESS
BLISTERING MAY OCCUR

INGESTION:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING: STOMACH PAINS

INDICATION OF IMMEDIATE MEDICAL ATTENTION AND SPECIAL TREATMENT NEEDED, IF
NECESSARY:

NOTES TO PHYSICIAN:
IN CASE OF INHALATION OF DECOMPOSITION PRODUCTS IN A FIRE, SYMPTOMS MAY BE
DELAYED. THE EXPOSED PERSON MAY NEED TO BE KEPT UNDER MEDICAL SURVEILLANCE
FOR 48 HOURS.

SPECIFIC TREATMENTS: NO SPECIFIC TREATMENT.

PROTECTION OF FIRST-AIDERS:
NO ACTION SHALL BE TAKEN INVOLVING ANY PERSONAL RISK OR WITHOUT SUITABLE
TRAINING. IF IT IS SUSPECTED THAT FUMES ARE STILL PRESENT, THE RESCUER
SHOULD WEAR AN APPROPRIATE MASK OR SELF-CONTAINED BREATHING APPARATUS.
IT MAY BE DANGEROUS TO THE PERSON PROVIDING AID TO GIVE MOUTH-TO-MOUTH
RESUSCITATION. WASH CONTAMINATED CLOTHING THOROUGHLY WITH WATER BEFORE
REMOVING IT, OR WEAR GLOVES.

SEE TOXICOLOGICAL INFORMATION (SECTION 11)


SECTION 5. FIRE-FIGHTING MEASURES 


EXTINGUISHING MEDIA:

SUITABLE EXTINGUISHING MEDIA:
USE AN EXTINGUISHING AGENT SUITABLE FOR THE SURROUNDING FIRE.

UNSUITABLE EXTINGUISHING MEDIA: NONE KNOWN.

SPECIFIC HAZARDS ARISING FROM THE CHEMICAL:
EXTREMELY FLAMMABLE AEROSOL. IN A FIRE OR IF HEATED, A PRESSURE INCREASE
WILL OCCUR AND THE CONTAINER MAY BURST, WITH THE RISK OF A SUBSEQUENT
EXPLOSION. GAS MAY ACCUMULATE IN LOW OR CONFINED AREAS OR TRAVEL A
CONSIDERABLE DISTANCE TO A SOURCE OF IGNITION AND FLASH BACK, CAUSING FIRE
OR EXPLOSION. BURSTING AEROSOL CONTAINERS MAY BE PROPELLED FROM A FIRE AT
HIGH SPEED. RUNOFF TO SEWER MAY CREATE FIRE OR EXPLOSION HAZARD.

HAZARDOUS THERMAL DECOMPOSITION PRODUCTS:
DECOMPOSITION PRODUCTS MAY INCLUDE THE FOLLOWING MATERIALS:
CARBON DIOXIDE
CARBON MONOXIDE
NITROGEN OXIDES
METAL OXIDE/OXIDES

SPECIAL PROTECTIVE ACTIONS FOR FIRE-FIGHTERS:
PROMPTLY ISOLATE THE SCENE BY REMOVING ALL PERSONS FROM THE VICINITY OF
THE INCIDENT IF THERE IS A FIRE. NO ACTION SHALL BE TAKEN INVOLVING ANY
PERSONAL RISK OR WITHOUT SUITABLE TRAINING. MOVE CONTAINERS FROM FIRE AREA
IF THIS CAN BE DONE WITHOUT RISK. USE WATER SPRAY TO KEEP FIRE-EXPOSED
CONTAINERS COOL.

SPECIAL PROTECTIVE EQUIPMENT FOR FIRE-FIGHTERS:
FIRE-FIGHTERS SHOULD WEAR APPROPRIATE PROTECTIVE EQUIPMENT AND
SELF-CONTAINED BREATHING APPARATUS (SCBA) WITH A FULL FACE-PIECE
OPERATED IN POSITIVE PRESSURE MODE.


SECTION 6. ACCIDENTAL RELEASE MEASURES 


PERSONAL PRECAUTIONS, PROTECTIVE EQUIPMENT AND EMERGENCY PROCEDURES:

FOR NON-EMERGENCY PERSONNEL:
NO ACTION SHALL BE TAKEN INVOLVING ANY PERSONAL RISK OR WITHOUT SUITABLE
TRAINING. EVACUATE SURROUNDING AREAS. KEEP UNNECESSARY AND UNPROTECTED
PERSONNEL FROM ENTERING. IN THE CASE OF AEROSOLS BEING RUPTURED, CARE
SHOULD BE TAKEN DUE TO THE RAPID ESCAPE OF THE PRESSURIZED CONTENTS AND
PROPELLANT. IF A LARGE NUMBER OF CONTAINERS ARE RUPTURED, TREAT AS A BULK
MATERIAL SPILLAGE ACCORDING TO THE INSTRUCTIONS IN THE CLEAN-UP SECTION. DO
NOT TOUCH OR WALK THROUGH SPILLED MATERIAL. SHUT OFF ALL IGNITION SOURCES.
NO FLARES, SMOKING OR FLAMES IN HAZARD AREA. DO NOT BREATHE VAPOR OR MIST.
PROVIDE ADEQUATE VENTILATION. WEAR APPROPRIATE RESPIRATOR WHEN VENTILATION
IS INADEQUATE. PUT ON APPROPRIATE PERSONAL PROTECTIVE EQUIPMENT.

FOR EMERGENCY RESPONDERS:
IF SPECIALISED CLOTHING IS REQUIRED TO DEAL WITH THE SPILLAGE, TAKE NOTE OF
ANY INFORMATION IN SECTION 8 ON SUITABLE AND UNSUITABLE MATERIALS. SEE ALSO
THE INFORMATION IN "FOR NON-EMERGENCY PERSONNEL".

ENVIRONMENTAL PRECAUTIONS:
AVOID DISPERSAL OF SPILLED MATERIAL AND RUNOFF AND CONTACT WITH SOIL,
WATERWAYS, DRAINS AND SEWERS. INFORM THE RELEVANT AUTHORITIES IF THE
PRODUCT HAS CAUSED ENVIRONMENTAL POLLUTION (SEWERS, WATERWAYS, SOIL OR
AIR).

METHODS AND MATERIALS FOR CONTAINMENT AND CLEANING UP:

SMALL SPILL:
STOP LEAK IF WITHOUT RISK. MOVE CONTAINERS FROM SPILL AREA. USE SPARK-PROOF
TOOLS AND EXPLOSION-PROOF EQUIPMENT. DILUTE WITH WATER AND MOP UP IF
WATER-SOLUBLE. ALTERNATIVELY, OR IF WATER-INSOLUBLE, ABSORB WITH AN INERT
DRY MATERIAL AND PLACE IN AN APPROPRIATE WASTE DISPOSAL CONTAINER. DISPOSE
OF VIA A LICENSED WASTE DISPOSAL CONTRACTOR.

LARGE SPILL:
STOP LEAK IF WITHOUT RISK. MOVE CONTAINERS FROM SPILL AREA. USE SPARK-PROOF
TOOLS AND EXPLOSION-PROOF EQUIPMENT. APPROACH RELEASE FROM UPWIND. PREVENT
ENTRY INTO SEWERS, WATER COURSES, BASEMENTS OR CONFINED AREAS. WASH
SPILLAGES INTO AN EFFLUENT TREATMENT PLANT OR PROCEED AS FOLLOWS. CONTAIN
AND COLLECT SPILLAGE WITH NON-COMBUSTIBLE, ABSORBENT MATERIAL E.G. SAND,
EARTH, VERMICULITE OR DIATOMACEOUS EARTH AND PLACE IN CONTAINER FOR
DISPOSAL ACCORDING TO LOCAL REGULATIONS (SEE SECTION 13). DISPOSE OF VIA A
LICENSED WASTE DISPOSAL CONTRACTOR. CONTAMINATED ABSORBENT MATERIAL MAY
POSE THE SAME HAZARD AS THE SPILLED PRODUCT.

NOTE:
SEE SECTION 1 FOR EMERGENCY CONTACT INFORMATION AND SECTION 13 FOR WASTE
DISPOSAL.


SECTION 7. HANDLING AND STORAGE 


PRECAUTIONS FOR SAFE HANDLING:

PROTECTIVE MEASURES:
PUT ON APPROPRIATE PERSONAL PROTECTIVE EQUIPMENT (SEE SECTION 8).

PRESSURIZED CONTAINER:
PROTECT FROM SUNLIGHT AND DO NOT EXPOSE TO TEMPERATURES EXCEEDING
50 DEG. C. DO NOT PIERCE OR BURN, EVEN AFTER USE. DO NOT GET IN EYES OR
ON SKIN OR CLOTHING. DO NOT BREATHE VAPOR OR MIST. DO NOT INGEST. AVOID
BREATHING GAS. USE ONLY WITH ADEQUATE VENTILATION. WEAR APPROPRIATE
RESPIRATOR WHEN VENTILATION IS INADEQUATE. STORE AND USE AWAY FROM HEAT,
SPARKS, OPEN FLAME OR ANY OTHER IGNITION SOURCE. USE EXPLOSION-PROOF
ELECTRICAL (VENTILATING, LIGHTING AND MATERIAL HANDLING) EQUIPMENT. USE
ONLY NON-SPARKING TOOLS. EMPTY CONTAINERS RETAIN PRODUCT RESIDUE AND CAN
BE HAZARDOUS.

ADVICE ON GENERAL OCCUPATIONAL HYGIENE:
EATING, DRINKING AND SMOKING SHOULD BE PROHIBITED IN AREAS WHERE THIS
MATERIAL IS HANDLED, STORED AND PROCESSED. WORKERS SHOULD WASH HANDS AND
FACE BEFORE EATING, DRINKING AND SMOKING. REMOVE CONTAMINATED CLOTHING AND
PROTECTIVE EQUIPMENT BEFORE ENTERING EATING AREAS. SEE ALSO SECTION 8 FOR
ADDITIONAL INFORMATION ON HYGIENE MEASURES.

CONDITIONS FOR SAFE STORAGE, INCLUDING ANY INCOMPATIBILITIES:
STORE IN ACCORDANCE WITH LOCAL REGULATIONS. STORE AWAY FROM DIRECT SUNLIGHT
IN A DRY, COOL AND WELL-VENTILATED AREA, AWAY FROM INCOMPATIBLE MATERIALS
(SEE SECTION 10) AND FOOD AND DRINK. PROTECT FROM SUNLIGHT. STORE LOCKED
UP. ELIMINATE ALL IGNITION SOURCES. USE APPROPRIATE CONTAINMENT TO AVOID
ENVIRONMENTAL CONTAMINATION.


SECTION 8. EXPOSURE CONTROLS/PERSONAL PROTECTION 


CONTROL PARAMETERS:

OCCUPATIONAL EXPOSURE LIMITS:

INGREDIENT NAME                       EXPOSURE LIMITS

BUTANE                                NIOSH REL (UNITED STATES, 10/2013).
                                      TWA: 800 PPM 10 HOURS.
                                      TWA: 1900 MG/M3 10 HOURS.

                                      ACGIH TLV (UNITED STATES, 4/2014).
                                      STEL: 1000 PPM 15 MINUTES.

2-BUTOXYETHANOL                       ACGIH TLV (UNITED STATES, 4/2014).
                                      TWA: 20 PPM 8 HOURS.

                                      NIOSH REL (UNITED STATES, 10/2013).
                                      ABSORBED THROUGH SKIN.
                                      TWA: 5 PPM 10 HOURS.
                                      TWA: 24 MG/M3 10 HOURS.

                                      OSHA PEL (UNITED STATES, 2/2013).
                                      ABSORBED THROUGH SKIN.
                                      TWA: 50 PPM 8 HOURS.
                                      TWA: 240 MG/M3 8 HOURS.

2-(2-ETHOXYETHOXY)-ETHANOL            AIHA WEEL (UNITED STATES, 10/2011).
                                      TWA: 25 PPM 8 HOURS.

PROPANE                               NIOSH REL (UNITED STATES, 10/2013).
                                      TWA: 1000 PPM 10 HOURS.
                                      TWA: 1800 MG/M3 10 HOURS.

                                      OSHA PEL (UNITED STATES, 2/2013).
                                      TWA: 1000 PPM 8 HOURS.
                                      TWA: 1800 MG/M3 8 HOURS.

APPROPRIATE ENGINEERING CONTROLS:
USE ONLY WITH ADEQUATE VENTILATION. IF USER OPERATIONS GENERATE DUST,
FUMES, GAS, VAPOR OR MIST, USE PROCESS ENCLOSURES, LOCAL EXHAUST
VENTILATION OR OTHER ENGINEERING CONTROLS TO KEEP WORKER EXPOSURE TO
AIRBORNE CONTAMINANTS BELOW ANY RECOMMENDED OR STATUTORY LIMITS. THE
ENGINEERING CONTROLS ALSO NEED TO KEEP GAS, VAPOR OR DUST CONCENTRATIONS
BELOW ANY LOWER EXPLOSIVE LIMITS. USE EXPLOSION-PROOF VENTILATION
EQUIPMENT.

ENVIRONMENTAL EXPOSURE CONTROLS:
EMISSIONS FROM VENTILATION OR WORK PROCESS EQUIPMENT SHOULD BE CHECKED
TO ENSURE THEY COMPLY WITH THE REQUIREMENTS OF ENVIRONMENTAL PROTECTION
LEGISLATION. IN SOME CASES, FUME SCRUBBERS, FILTERS OR ENGINEERING
MODIFICATIONS TO THE PROCESS EQUIPMENT WILL BE NECESSARY TO REDUCE
EMISSIONS TO ACCEPTABLE LEVELS.

INDIVIDUAL PROTECTION MEASURES:

HYGIENE MEASURES:
WASH HANDS, FOREARMS AND FACE THOROUGHLY AFTER HANDLING CHEMICAL PRODUCTS,
BEFORE EATING, SMOKING AND USING THE LAVATORY AND AT THE END OF THE WORKING
PERIOD. APPROPRIATE TECHNIQUES SHOULD BE USED TO REMOVE POTENTIALLY
CONTAMINATED CLOTHING. WASH CONTAMINATED CLOTHING BEFORE REUSING. ENSURE
THAT EYEWASH STATIONS AND SAFETY SHOWERS ARE CLOSE TO THE WORKSTATION
LOCATION.

EYE/FACE PROTECTION:
SAFETY EYEWEAR COMPLYING WITH AN APPROVED STANDARD SHOULD BE USED WHEN A
RISK ASSESSMENT INDICATES THIS IS NECESSARY TO AVOID EXPOSURE TO LIQUID
SPLASHES, MISTS, GASES OR DUSTS.

IF CONTACT IS POSSIBLE, THE FOLLOWING PROTECTION SHOULD BE WORN, UNLESS
THE ASSESSMENT INDICATES A HIGHER DEGREE OF PROTECTION:
CHEMICAL SPLASH GOGGLES AND/OR FACE SHIELD. IF INHALATION HAZARDS EXIST, A
FULL-FACE RESPIRATOR MAY BE REQUIRED INSTEAD.

SKIN PROTECTION:

HAND PROTECTION:
CHEMICAL-RESISTANT, IMPERVIOUS GLOVES COMPLYING WITH AN APPROVED STANDARD
SHOULD BE WORN AT ALL TIMES WHEN HANDLING CHEMICAL PRODUCTS IF A RISK
ASSESSMENT INDICATES THIS IS NECESSARY. CONSIDERING THE PARAMETERS
SPECIFIED BY THE GLOVE MANUFACTURER, CHECK DURING USE THAT THE GLOVES ARE
STILL RETAINING THEIR PROTECTIVE PROPERTIES. IT SHOULD BE NOTED THAT THE
TIME TO BREAKTHROUGH FOR ANY GLOVE MATERIAL MAY BE DIFFERENT FOR DIFFERENT
GLOVE MANUFACTURERS. IN THE CASE OF MIXTURES, CONSISTING OF SEVERAL
SUBSTANCES, THE PROTECTION TIME OF THE GLOVES CANNOT BE ACCURATELY
ESTIMATED.

BODY PROTECTION:
PERSONAL PROTECTIVE EQUIPMENT FOR THE BODY SHOULD BE SELECTED BASED ON THE
TASK BEING PERFORMED AND THE RISKS INVOLVED AND SHOULD BE APPROVED BY A
SPECIALIST BEFORE HANDLING THIS PRODUCT. WHEN THERE IS A RISK OF IGNITION
FROM STATIC ELECTRICITY, WEAR ANTISTATIC PROTECTIVE CLOTHING. FOR THE
GREATEST PROTECTION FROM STATIC DISCHARGES, CLOTHING SHOULD INCLUDE
ANTI-STATIC OVERALLS, BOOTS AND GLOVES.

OTHER SKIN PROTECTION:
APPROPRIATE FOOTWEAR AND ANY ADDITIONAL SKIN PROTECTION MEASURES SHOULD BE
SELECTED BASED ON THE TASK BEING PERFORMED AND THE RISKS INVOLVED AND
SHOULD BE APPROVED BY A SPECIALIST BEFORE HANDLING THIS PRODUCT.

RESPIRATORY PROTECTION:
USE A PROPERLY FITTED, AIR-PURIFYING OR AIR-FED RESPIRATOR COMPLYING WITH
AN APPROVED STANDARD IF A RISK ASSESSMENT INDICATES THIS IS NECESSARY.
RESPIRATOR SELECTION MUST BE BASED ON KNOWN OR ANTICIPATED EXPOSURE LEVELS,
THE HAZARDS OF THE PRODUCT AND THE SAFE WORKING LIMITS OF THE SELECTED
RESPIRATOR.


SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE:

PHYSICAL STATE: LIQUID.

COLOR: NOT AVAILABLE.

ODOR: NOT AVAILABLE.

ODOR THRESHOLD: NOT AVAILABLE.

PH: 13

MELTING POINT: NOT AVAILABLE.

BOILING POINT: NOT AVAILABLE.

FLASH POINT:
CLOSED CUP: -29 DEG. C (-20.2 DEG. F) [PENSKY-MARTENS CLOSED CUP]

EVAPORATION RATE: 0.09 (BUTYL ACETATE = 1)

FLAMMABILITY (SOLID, GAS): NOT AVAILABLE.

LOWER AND UPPER EXPLOSIVE (FLAMMABLE) LIMITS:
LOWER: 1.1%
UPPER: 23.5%

VAPOR PRESSURE: 13.5 KPA (101.325 MMHg) [AT 20 DEG. C]

VAPOR DENSITY: 1 [AIR = 1]

RELATIVE DENSITY: 0.97

SOLUBILITY: NOT AVAILABLE.

PARTITION COEFFICIENT N-OCTANOL/WATER: NOT AVAILABLE.

AUTO-IGNITION TEMPERATURE: NOT AVAILABLE.

DECOMPOSITION TEMPERATURE: NOT AVAILABLE.

VISCOSITY:
KINEMATIC (ROOM TEMPERATURE): >0.205 CM2/S (>20.5 CST)
KINEMATIC (40 DEG. C (104 DEG. F)): >0.205 CM2/S (>20.5 CST)

AEROSOL PRODUCT:
TYPE OF AEROSOL: SPRAY
HEAT OF COMBUSTION: 0.000004589 KJ/G


SECTION 10. STABILITY AND REACTIVITY 


REACTIVITY:
NO SPECIFIC TEST DATA RELATED TO REACTIVITY AVAILABLE FOR THIS PRODUCT OR
ITS INGREDIENTS.

CHEMICAL STABILITY: THE PRODUCT IS STABLE.

POSSIBILITY OF HAZARDOUS REACTIONS:
UNDER NORMAL CONDITIONS OF STORAGE AND USE, HAZARDOUS REACTIONS WILL NOT
OCCUR.

CONDITIONS TO AVOID:
AVOID ALL POSSIBLE SOURCES OF IGNITION (SPARK OR FLAME).

INCOMPATIBLE MATERIALS: NO SPECIFIC DATA.

HAZARDOUS DECOMPOSITION PRODUCTS:
UNDER NORMAL CONDITIONS OF STORAGE AND USE, HAZARDOUS DECOMPOSITION
PRODUCTS SHOULD NOT BE PRODUCED.


SECTION 11. TOXICOLOGICAL INFORMATION 


INFORMATION ON TOXICOLOGICAL EFFECTS:

ACUTE TOXICITY:

PRODUCT/INGREDIENT  RESULT             SPECIES     DOSE           EXPOSURE
NAME

BUTANE              LC50 INHALATION    RAT         658000 MG/M3   4 HOURS
                    VAPOR

2-BUTOXYETHANOL     LCLO INHALATION    GUINEA PIG  >3.1 MG/L      1 HOURS
                    VAPOR

                    LD50 DERMAL        GUINEA PIG  >2000 MG/KG

                    LD50 ORAL          RAT         1300 MG/KG

2-(2-ETHOXY-        LD50 ORAL          RAT         7500 MG/KG
ETHOXY)-ETHANOL

TETRASODIUM         LD50 ORAL          RAT         10 G/KG
ETHYLENE DIAMINE
TETRAACETATE

IRRITATION/CORROSION:

PRODUCT/      RESULT         SPECIES  SCORE  EXPOSURE           OBSERVATION
INGREDIENT
NAME

2-BUTOXY-     EYES:          RABBIT          24 HOURS
ETHANOL       MODERATE                       100 MILLIGRAMS
              IRRITANT

              EYES:          RABBIT          100 MILLIGRAMS
              SEVERE
              IRRITANT

              SKIN:          RABBIT          500 MILLIGRAMS
              MILD IRRITANT

2-(2-ETHOXY-  EYES:          RABBIT          125 MILLIGRAMS
ETHOXY)-      MILD IRRITANT
ETHANOL
              EYES:          RABBIT          500 MILLIGRAMS
              MODERATE
              IRRITANT

              SKIN:          RABBIT          24 HOURS
              MILD IRRITANT                  500 MILLIGRAMS

TETRASODIUM   EYES:          RABBIT:         24 HOURS
ETHYLENE      MODERATE                       100 MILLIGRAMS
DIAMINE       IRRITANT
TETRAACETATE
              SKIN:          RABBIT          24 HOURS
              MODERATE                       500 MILLIGRAMS
              IRRITANT

SENSITIZATION: NOT AVAILABLE.

MUTAGENICITY: NOT AVAILABLE.

CARCINOGENICITY: NOT AVAILABLE.

CLASSIFICATION:

PRODUCT/INGREDIENT NAME        OSHA      IARC       NTP

2-BUTOXYETHANOL                          3

REPRODUCTIVE TOXICITY: NOT AVAILABLE.

TERATOGENICITY: NOT AVAILABLE.

SPECIFIC TARGET ORGAN TOXICITY (SINGLE EXPOSURE):

NAME                    CATEGORY      ROUTE OF          TARGET ORGANS
                                      EXPOSURE

BUTANE                  CATEGORY 3    NOT APPLICABLE.   RESPIRATORY TRACT
                                                        IRRITATION AND
                                                        NARCOTIC EFFECTS

2-BUTOXYETHANOL         CATEGORY 3    NOT APPLICABLE.   RESPIRATORY TRACT
                                                        IRRITATION AND
                                                        NARCOTIC EFFECTS

2-(2-ETHOXYETHOXY)-     CATEGORY 3    NOT APPLICABLE.   RESPIRATORY TRACT
ETHANOL                                                 IRRITATION AND
                                                        NARCOTIC EFFECTS

PROPANE                 CATEGORY 3    NOT APPLICABLE.   RESPIRATORY TRACT
                                                        IRRITATION AND
                                                        NARCOTIC EFFECTS

SPECIFIC TARGET ORGAN TOXICITY (REPEATED EXPOSURE):

NAME                    CATEGORY      ROUTE OF          TARGET ORGANS
                                      EXPOSURE

BUTANE                  CATEGORY 2    NOT DETERMINED    NOT DETERMINED

2-BUTOXYETHANOL         CATEGORY 2    NOT DETERMINED    NOT DETERMINED

2-(2-ETHOXYETHOXY)-     CATEGORY 2    NOT DETERMINED    NOT DETERMINED
ETHANOL

PROPANE                 CATEGORY 2    NOT DETERMINED    NOT DETERMINED

ASPIRATION HAZARD:

NAME                         RESULT

BUTANE                       ASPIRATION HAZARD - CATEGORY 1

PROPANE                      ASPIRATION HAZARD - CATEGORY 1

INFORMATION ON THE LIKELY ROUTES OF EXPOSURE: NOT AVAILABLE.

POTENTIAL ACUTE HEALTH EFFECTS:

EYE CONTACT: CAUSES SERIOUS EYE DAMAGE.

INHALATION:
MAY GIVE OFF GAS, VAPOR OR DUST THAT IS VERY IRRITATING OR CORROSIVE TO THE
RESPIRATORY SYSTEM. EXPOSURE TO DECOMPOSITION PRODUCTS MAY CAUSE A HEALTH
HAZARD. SERIOUS EFFECTS MAY BE DELAYED FOLLOWING EXPOSURE.

SKIN CONTACT: CAUSES SEVERE BURNS.

INGESTION: MAY CAUSE BURNS TO MOUTH, THROAT AND STOMACH.

SYMPTOMS RELATED TO THE PHYSICAL, CHEMICAL AND TOXICOLOGICAL
CHARACTERISTICS:

EYE CONTACT:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
PAIN
WATERING
REDNESS

INHALATION:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
RESPIRATORY TRACT IRRITATION
COUGHING

SKIN CONTACT:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING:
PAIN OR IRRITATION
REDNESS
BLISTERING MAY OCCUR

INGESTION:
ADVERSE SYMPTOMS MAY INCLUDE THE FOLLOWING: STOMACH PAINS

DELAYED AND IMMEDIATE EFFECTS AND ALSO CHRONIC EFFECTS FROM SHORT AND LONG
TERM EXPOSURE:

SHORT TERM EXPOSURE:
POTENTIAL IMMEDIATE EFFECTS: NOT AVAILABLE.
POTENTIAL DELAYED EFFECTS: NOT AVAILABLE.

LONG TERM EXPOSURE:
POTENTIAL IMMEDIATE EFFECTS: NOT AVAILABLE.
POTENTIAL DELAYED EFFECTS: NOT AVAILABLE.

POTENTIAL CHRONIC HEALTH EFFECTS: NOT AVAILABLE.

GENERAL: MAY CAUSE DAMAGE TO ORGANS THROUGH PROLONGED OR REPEATED EXPOSURE.

CARCINOGENICITY: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.

MUTAGENICITY: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.

TERATOGENICITY: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.

DEVELOPMENTAL EFFECTS: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.

FERTILITY EFFECTS: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.

NUMERICAL MEASURES OF TOXICITY:

ACUTE TOXICITY ESTIMATES:

ROUTE                     ATE VALUE

ORAL                      21502.3 MG/KG


SECTION 12. ECOLOGICAL INFORMATION 


TOXICITY:

PRODUCT/INGREDIENT  RESULT                SPECIES                  EXPOSURE
NAME

2-BUTOXYETHANOL     ACUTE EC50:           DAPHNIA - DAPHNIA MAGNA  48 HOURS
                    >1000 MG/L
                    FRESH WATER

                    ACUTE LC50:           CRUSTACEANS - CRANGON    48 HOURS
                    800000 (MICRO)G/L     CRANGON
                    MARINE WATER

                    ACUTE LC50:           FISH - MENIDIA           96 HOURS
                    1250000 (MICRO)G/L    BERYLLINA
                    MARINE WATER

2-(2-ETHOXY-        ACUTE LC50:           DAPHNIA - DAPHNIA        48 HOURS
ETHOXY)-ETHANOL     3340000 (MICRO)G/L    MAGNA - NEONATE
                    FRESH WATER

                    ACUTE LC50:           FISH - ICTALURUS         96 HOURS
                    6010000 (MICRO)G/L    PUNCTATUS
                    FRESH WATER

TETRASODIUM         ACUTE LC50:           FISH - LEPOMIS           96 HOURS
ETHYLENE DIAMINE    486000 (MICRO)G/L     MACROCHIRUS
TETRAACETATE        FRESH WATER

PERSISTENCE AND DEGRADABILITY:

PRODUCT/INGREDIENT NAME   AQUATIC HALF-LIFE   PHOTOLYSIS   BIODEGRADABILITY

2-BUTOXYETHANOL                                            READILY

BIOACCUMULATIVE POTENTIAL:

PRODUCT/INGREDIENT NAME             LOGPOW      BCF       POTENTIAL

TETRASODIUM ETHYLENE DIAMINE                    1.8       LOW
TETRAACETATE

MOBILITY IN SOIL:
SOIL/WATER PARTITION COEFFICIENT (KOC): NOT AVAILABLE.

OTHER ADVERSE EFFECTS: NO KNOWN SIGNIFICANT EFFECTS OR CRITICAL HAZARDS.


SECTION 13. DISPOSAL CONSIDERATIONS 


DISPOSAL METHODS:
THE GENERATION OF WASTE SHOULD BE AVOIDED OR MINIMIZED WHEREVER POSSIBLE.
DISPOSAL OF THIS PRODUCT, SOLUTIONS AND ANY BY-PRODUCTS SHOULD AT ALL TIMES
COMPLY WITH THE REQUIREMENTS OF ENVIRONMENTAL PROTECTION AND WASTE DISPOSAL
LEGISLATION AND ANY REGIONAL LOCAL AUTHORITY REQUIREMENTS. DISPOSE OF
SURPLUS AND NON-RECYCLABLE PRODUCTS VIA A LICENSED WASTE DISPOSAL
CONTRACTOR. WASTE SHOULD NOT BE DISPOSED OF UNTREATED TO THE SEWER UNLESS
FULLY COMPLIANT WITH THE REQUIREMENTS OF ALL AUTHORITIES WITH JURISDICTION.
WASTE PACKAGING SHOULD BE RECYCLED. INCINERATION OR LANDFILL SHOULD ONLY BE
CONSIDERED WHEN RECYCLING IS NOT FEASIBLE. THIS MATERIAL AND ITS CONTAINER
MUST BE DISPOSED OF IN A SAFE WAY. EMPTY CONTAINERS OR LINERS MAY RETAIN
SOME PRODUCT RESIDUES. DO NOT PUNCTURE OR INCINERATE CONTAINER.


SECTION 14. TRANSPORT INFORMATION 


                            DOT              TDG             MEXICO
                            CLASSIFICATION   CLASSIFICATION  CLASSIFICATION

UN NUMBER                   UN1950           UN1950          UN1950

UN PROPER SHIPPING NAME     AEROSOLS         AEROSOLS        AEROSOLS

TRANSPORT HAZARD CLASS(ES)  2.2              2.2             2.2

                            NON-FLAMMABLE    CLASS 2.2,      CLASS 2.2,
                            GAS, CLASS/      NON-FLAMMABLE   NON-FLAMMABLE
                            DIVISION 2.2     AND NON-TOXIC   AND NON-TOXIC
                                             GASES           GASES

PACKING GROUP

ENVIRONMENTAL HAZARDS       NO.              NO.             NO.

ADDITIONAL INFORMATION      SPECIAL          SPECIAL         SPECIAL
                            PROVISIONS:      PROVISIONS:     PROVISIONS:
                            LIMITED          LIMITED         (ERG#126)
                            QUANTITY         QUANTITY


                              IATA                   IMDG

UN NUMBER                     UN1950                 UN1950

UN PROPER SHIPPING NAME       AEROSOLS,              AEROSOLS
                              NON-FLAMMABLE

TRANSPORT HAZARD CLASS(ES)    2.2                    2.2

                              CLASS 2.2,             CLASS 2.2 -
                              NON-FLAMMABLE          NON-FLAMMABLE GASES
                              AND NON-TOXIC GASES

PACKING GROUP

ENVIRONMENTAL HAZARDS         NO.                    NO.

ADDITIONAL INFORMATION        SPECIAL PROVISIONS:    EMERGENCY SCHEDULES
                              LIMITED QUANTITY       (EMS):
                                                     LIMITED QUANTITY,
                                                     F-D, S-U

SPECIAL PRECAUTIONS FOR USER:
MULTI-MODAL SHIPPING DESCRIPTIONS ARE PROVIDED FOR INFORMATIONAL PURPOSES
AND DO NOT CONSIDER CONTAINER SIZES. THE PRESENCE OF A SHIPPING DESCRIPTION
FOR A PARTICULAR MODE OF TRANSPORT (SEA, AIR, ETC.), DOES NOT INDICATE THAT
THE PRODUCT IS PACKAGED SUITABLY FOR THAT MODE OF TRANSPORT. ALL PACKAGING
MUST BE REVIEWED FOR SUITABILITY PRIOR TO SHIPMENT, AND COMPLIANCE WITH THE
APPLICABLE REGULATIONS IS THE SOLE RESPONSIBILITY OF THE PERSON OFFERING
THE PRODUCT FOR TRANSPORT. PEOPLE LOADING AND UNLOADING DANGEROUS GOODS
MUST BE TRAINED ON ALL OF THE RISKS DERIVING FROM THE SUBSTANCES AND ON ALL
ACTIONS IN CASE OF EMERGENCY SITUATIONS.

TRANSPORT IN BULK ACCORDING TO ANNEX II OF MARPOL 73/78 AND THE IBC CODE:
NOT AVAILABLE.


SECTION 15. REGULATORY INFORMATION 


U.S. FEDERAL REGULATIONS:

STATE REGULATIONS:

CALIFORNIA PROP. 65:

WARNING:
THIS PRODUCT CONTAINS CHEMICALS KNOWN TO THE STATE OF CALIFORNIA TO CAUSE
CANCER AND BIRTH DEFECTS OR OTHER REPRODUCTIVE HARM.


SECTION 16. OTHER INFORMATION 


HAZARDOUS MATERIAL INFORMATION SYSTEM (U.S.A.):
HEALTH           2
FLAMMABILITY     2
PHYSICAL HAZARDS 0

CAUTION:
HMIS(R*) RATINGS ARE BASED ON A 0-4 RATING SCALE, WITH 0 REPRESENTING
MINIMAL HAZARDS OR RISKS, AND 4 REPRESENTING SIGNIFICANT HAZARDS OR RISKS
ALTHOUGH HMIS(R*) RATINGS ARE NOT REQUIRED ON SDSS UNDER 29 CFR 1910.1200,
THE PREPARER MAY CHOOSE TO PROVIDE THEM. HMIS(R*) RATINGS ARE TO BE USED
WITH A FULLY IMPLEMENTED HMIS(R*) PROGRAM. HMIS(R*) IS A REGISTERED MARK
OF THE NATIONAL PAINT & COATINGS ASSOCIATION (NPCA). HMIS(R*) MATERIALS
MAY BE PURCHASED EXCLUSIVELY FROM J. J. KELLER (800) 327-6868.

THE CUSTOMER IS RESPONSIBLE FOR DETERMINING THE PPE CODE FOR THIS MATERIAL.

NOTICE TO READER:
IT IS RECOMMENDED THAT EACH CUSTOMER OR RECIPIENT OF THIS SAFETY DATA SHEET
(SDS) STUDY IT CAREFULLY AND CONSULT RESOURCES, AS NECESSARY OR
APPROPRIATE, TO BECOME AWARE OF AND UNDERSTAND THE DATA CONTAINED IN THIS
SDS AND ANY HAZARDS ASSOCIATED WITH THE PRODUCT. THIS INFORMATION IS
PROVIDED IN GOOD FAITH AND BELIEVED TO BE ACCURATE AS OF THE EFFECTIVE DATE
HEREIN. HOWEVER, NO WARRANTY, EXPRESS OR IMPLIED, IS GIVEN. THE INFORMATION
PRESENTED HERE APPLIES ONLY TO THE PRODUCT AS SHIPPED. THE ADDITION OF ANY
MATERIAL CAN CHANGE THE COMPOSITION, HAZARDS AND RISKS OF THE PRODUCT.
REGULATORY REQUIREMENTS ARE SUBJECT TO CHANGE AND MAY DIFFER BETWEEN
VARIOUS LOCATIONS AND JURISDICTIONS. THE CUSTOMER/BUYER/USER IS RESPONSIBLE
TO ENSURE THAT HIS ACTIVITIES COMPLY WITH ALL COUNTRY, FEDERAL, STATE,
PROVINCIAL OR LOCAL LAWS. THE CONDITIONS FOR USE OF THE PRODUCT ARE NOT
UNDER THE CONTROL OF THE MANUFACTURER; THE CUSTOMER/BUYER/USER IS
RESPONSIBLE TO DETERMINE THE CONDITIONS NECESSARY FOR THE SAFE USE OF THIS
PRODUCT. THE CUSTOMER/BUYER/USER SHOULD NOT USE THE PRODUCT FOR ANY PURPOSE
OTHER THAN THE PURPOSE SHOWN IN THE APPLICABLE SECTION OF THIS SDS WITHOUT
FIRST REFERRING TO THE SUPPLIER AND OBTAINING WRITTEN HANDLING
INSTRUCTIONS. DUE TO THE PROLIFERATION OF SOURCES FOR INFORMATION SUCH AS
MANUFACTURER-SPECIFIC SDS, THE MANUFACTURER CANNOT BE RESPONSIBLE FOR SDSS
OBTAINED FROM ANY OTHER SOURCE.

DATE OF ISSUE/DATE OF REVISION: 5/22/2015.

DATE OF PREVIOUS ISSUE: NO PREVIOUS VALIDATION.

VERSION: 1