Common Name: LITHIUM-ION RECHARGEABLE BATTERY PACK, BL1830
Manufacturer: MAKITA
SDS Revision Date: 8/3/2016
SDS Format: ANSI-OSHA
   
Item Number(s): 12M837, 13P059, 13P060, 13P061, 14F046, 14F055, 14F056, 14F057, 14F058, 14F059, 14F060, 14F062, 14F063, 14F074, 14F075, 14F076, 14F077, 14F078, 14F079, 14F145, 14F146, 14F154, 14F155, 14F156, 14F157, 14F158, 14F159, 14F160, 14F161, 14F162, 14F163, 14F164, 15X778, 15X779, 15X813, 15X814, 15X815, 20JX63, 20KR54, 20KR56, 20KR59, 20UJ15, 20UJ17, 20UJ19, 20UJ20, 20UJ24, 21R986, 21R987, 21R990, 21TX97, 22EN59, 22P217, 22P228, 22P229, 22P231, 22P232, 22UT87, 22UT89, 22UT90, 22UT91, 22UT92, 22UT93, 22UT94, 22UT95, 22UT96, 22UT97, 23X911, 31HJ80, 31HJ81, 31HJ82, 31HJ83, 31HJ84, 31HJ85, 31HJ86, 31HJ87, 31HJ88, 31HJ89, 31HJ90, 31HJ91, 33RT41, 33RT42, 33RT43, 33RT44, 34G793, 34G795, 34G797, 34G799, 34G805, 39D699, 39D715, 40H693, 40K958, 40K960, 40K965, 40K992, 40K993, 45L121, 49U820, 4MGW5, 4NNH6, 4NNH7, 4NNH8, 4NNH9, 4NNJ1, 4NNJ2, 4NNJ3, 4NNJ4, 4NNJ5, 4NNJ6, 4NNJ7, 4NNJ8, 4NNJ9, 4NNK1, 4NNK2, 4NNK3, 4NNK4, 4NNK5, 4NNK6, 4NNK7, 4NNK8, 4NNK9, 4NNL1, 4NNL2, 4NNL3, 4NNL4, 4NNL5, 4NNL6, 4NNL7, 4NNL8, 4NNL9, 4NNN1, 4NNN2, 4NNN4, 4NNN5, 4NNN8, 4NNN9, 4NNP1, 4NNP2, 6CCJ3, 6CCJ4, 6CCJ7, 6CFA8, 6CFA9, 6CFC0, 6CFC1, 6CFC2, 6CFC3, 6CFC4, 6CFC5, 6MRP9, 6MRR0, 6XZU6, 9VNH9
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1. CHEMICAL PRODUCT AND COMPANY NAME 
SECTION 2. HAZARD IDENTIFICATION 
SECTION 3. COMPOSITION, INFORMATION OR INGREDIENTS 
SECTION 4. FIRST AID MEASURE 
SECTION 5. FIRE FIGHTING MEASURES 
SECTION 6. ACCIDENTAL RELEASE MEASURES 
SECTION 7. HANDLING AND STORAGE 
SECTION 8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 
SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10. STABILITY AND REACTIVITY 
SECTION 11. TOXICOLOGICAL INFORMATION 
SECTION 12. ECOLOGICAL INFORMATION 
SECTION 13. DISPOSAL CONSIDERATIONS 
SECTION 14. TRANSPORT INFORMATION 
SECTION 15. REGULATORY INFORMATION 
SECTION 16. OTHER INFORMATION 



SAFETY DATA SHEET

COMPLIES WITH THE OSHA HAZARD COMMUNICATION STANDARD: 29 CFR 1910 1200


SECTION 1. CHEMICAL PRODUCT AND COMPANY NAME 


LITHIUM-ION RECHARGEABLE BATTERY PACK BL1830

MAKITA U.S.A., INC.
14930-C NORTHAM STREET
LA MIRADA, CA 90638

PREPARED BY: STAN RODRIGUES

DATE REVISED: 08/03/2016

EMERGENCY CONTACT INFORMATION:

TELEPHONE NUMBER FOR INFORMATION:
MAKITA: 1-510-657-9881

EMERGENCY RESPONSE:

FOR CHEMICAL EMERGENCY SPILLS, LEAK, FIRE, EXPOSURE, OR ACCIDENT CALL
CHEMTREC DAY OR NIGHT WITHIN USA AND CANADA: 1-800-424-9300


SECTION 2. HAZARD IDENTIFICATION 


CLASS NAME: NOT APPLICABLE FOR REGULATED CLASS

HAZARD:
IT MAY CAUSE HEAT GENERATION OR ELECTROLYTE LEAKAGE IF BATTERY TERMINALS
CONTACT WITH OTHER METALS. ELECTROLYTE IS FLAMMABLE. IN CASE OF ELECTROLYTE
LEAKAGE, MOVE THE BATTERY FROM FIRE IMMEDIATELY.

TOXICITY:
VAPOR GENERATED FROM BURNING BATTERIES, MAY MAKE EYES, SKIN AND THROAT
IRRITATE.


SECTION 3. COMPOSITION, INFORMATION OR INGREDIENTS 


IMPORTANT NOTE:

THE BATTERY PACK SHOULD NOT BE OPENED OR BURNED SINCE THE FOLLOWING
INGREDIENTS CONTAINED WITHIN THE CELL THAT COULD BE HARMFUL UNDER SOME
CIRCUMSTANCE IF EXPOSED OR MISUSED.

THE CELL CONTAINS NEITHER METALLIC LITHIUM NOR LITHIUM ALLOY.

CATHODE:
LITHIUM NICKEL COBALT MANGANESE OXIDES (ACTIVE MATERIAL)
POLYVINYLIDENE FLUORIDE (BINDER)
GRAPHITE (CONDUCTIVE MATERIAL)

ANODE:
GRAPHITE (ACTIVE MATERIAL)
POLYVINYLIDENE FLUORIDE (BINDER)

ELECTROLYTE:
ORGANIC SOLVENT (NON-AQUEOUS LIQUID)
LITHIUM SALT

OTHERS:
HEAVY METALS SUCH AS MERCURY, CADMIUM, LEAD, AND CHROMIUM ARE NOT USED IN
THE CELL.

ENCLOSURE: PLASTIC (PC)

UN NUMBER: UN3480

WATT-HOUR RATING: 54WH FOR BATTERY PACK


SECTION 4. FIRST AID MEASURE 


THE PRODUCT CONTAINS ORGANIC ELECTROLYTE. IN CASE OF ELECTROLYTE LEAKAGE
FORM THE BATTERY, ACTIONS DESCRIBED BELOW ARE REQUIRED.

EYE CONTACT:
FLUSH THE EYES WITH PLENTY OF CLEAN WATER FOR AT LEAST 15 MINUTES
IMMEDIATELY, WITHOUT RUBBING, AND CALL A DOCTOR. IF APPROPRIATE PROCEDURES
ARE NOT TAKEN; THIS MAY CAUSE AN EYE IRRITATION.

SKIN CONTACT:
WASH THE CONTACT AREAS OFF IMMEDIATELY WITH PLENTY OF WATER AND SOAP. IF
APPROPRIATE PROCEDURES ARE NOT TAKEN, THIS MAY CAUSE SORES ON THE SKIN.

INHALATION: REMOVE TO FRESH AIR IMMEDIATELY, AND CALL A DOCTOR.


SECTION 5. FIRE FIGHTING MEASURES 


USE SPECIFIED EXTINGUISHERS (GAS, FOAM, POWDER) AND EXTINGUISHING SYSTEM
UNDER THE FIRE DEFENSE LAW.

SINCE CORROSIVE GAS MAY BE PRODUCED AT THE TIME OF FIRE EXTINGUISHING, USE
AN AIR INHALATOR WHEN DANGER IS PREDICTED.

USE A LARGE AMOUNT OF WATER AS A SUPPORTIVE MEASURE IN ORDER TO GET COOLING
EFFECT IF NEEDED. (INDOOR/OUTDOOR FIRE HYDRANT)

CARRY AWAY FLAMMABLE MATERIALS IMMEDIATELY IN CASE OF FIRE.

MOVE BATTERIES TO A SAFER PLACE IMMEDIATELY IN CASE OF FIRE.


SECTION 6. ACCIDENTAL RELEASE MEASURES 


WIPE OFF WITH DRY CLOTH

KEEP AWAY FROM FIRE

WEAR SAFETY GOGGLES, SAFETY GLOVES AS NEEDED


SECTION 7. HANDLING AND STORAGE 


STORAGE:
STORE WITHIN THE RECOMMENDED LIMIT OF -30 DEG. C TO 45 DEG. C (-22 DEG. F
TO 113 DEG. F), WELL-VENTILATED AREA. DO NOT EXPOSE TO HIGH TEMPERATURE (60
DEG. C/140 DEG. F). SINCE SHORT CIRCUIT CAN CAUSE BUM HAZARD OR SAFETY VENT
TO OPEN, DO NOT STORE WITH METAL JEWELRY, METAL COVERED TABLES, OR METAL
BELT.

HANDLING:

DO NOT DISASSEMBLE, ALTER, OR SOLDER. DO NOT SHORT + AND - TERMINALS WITH
METAL.

DO NOT OPEN THE BATTERY PACK.

CHARGING:
CHARGE WITHIN THE LIMITS OF 0 DEG. C TO 40 DEG. C (32 DEG. F TO 104 DEG. F)
TEMPERATURE. CHARGE WITH SPECIFIED CHARGER DESIGNED FOR THIS BATTERY PACK

DISCHARGING:
DISCHARGE WITHIN THE LIMITS OF -20 DEG. C TO 60 DEG. C (-4 DEG. F TO 140
DEG. F) TEMPERATURE.

DISPOSAL:
DISPOSE IN ACCORDANCE WITH APPLICABLE FEDERAL, STATE AND LOCAL REGULATIONS.

CAUTION:
FOR SAFE OPERATION, SEE INSTRUCTION MANUAL. USE ONLY WITH MAKITA HIGH
CAPACITY CHARGER. CHARGING ROOM TEMP.: 10 DEG. C - 40 DEG. C. DO NOT EXPOSE
BATTERY TO WATER OR RAIN. DO NOT DESTROY BATTERY BY FIRE.


SECTION 8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 


(IN CASE ELECTROLYTE IS LEAKED FROM BATTERY)

ACCEPTABLE CONCENTRATION: NOT SPECIFIED IN ACGIH.

FACILITIES:
PROVIDE APPROPRIATE VENTILATION SUCH AS LOCAL VENTILATION SYSTEM IN THE
STORAGE.

PROTECTIVE CLOTHING:
GAS MASK FOR ORGANIC GASES, SAFETY GOGGLE, SAFETY GLOVE.


SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: LITHIUM-ION RECHARGEABLE CELLS ARE SET IN A RESIN CASE.

AVERAGE OPERATING VOLTAGE: 18V


SECTION 10. STABILITY AND REACTIVITY 


EXTERNAL SHORT-CIRCUIT, DEFORMATION BY CRUSH, HIGH TEMPERATURE (OVER 100
DEG. C) EXPOSURE OF THE BATTERY MAY CAUSE GENERATION OF HEAT AND IGNITION.


SECTION 11. TOXICOLOGICAL INFORMATION 


ACUTE TOXICITY: NO INFORMATION AS A BATTERY

LOCAL EFFECTS: NO INFORMATION AS A BATTERY


SECTION 12. ECOLOGICAL INFORMATION 


IF BATTERY IS BURIED IN THE GROUND, CORROSION MAY OCCUR ON THE OUTER
PLASTIC CASE OF BATTERY AND THE ELECTROLYTE MAY LEAK OUT. THERE IS NO
INFORMATION ON ENVIRONMENTAL INFLUENCE.


SECTION 13. DISPOSAL CONSIDERATIONS 


WHEN BATTERY IS DISPOSED, ISOLATE POSITIVE (+) AND NEGATIVE (-) TERMINALS
OF THE BATTERY TO AVOID THOSE TERMINALS FROM TOUCHING EACH OTHER. BATTERIES
MAY BE SHORT-CIRCUITED WHEN PILED UP OR MIXED WITH THE OTHER BATTERIES.
DISPOSE IN ACCORDANCE WITH APPLICABLE FEDERAL, STATE AND LOCAL REGULATIONS.


SECTION 14. TRANSPORT INFORMATION 


THE CELLS IN THESE BATTERIES HAVE BEEN TESTED AND MEET THE REQUIREMENTS FOR
THE UN MANUAL OF TESTS AND CRITERIA, PART III, SUBSECTION 38.3.

WHEN A NUMBER OF BATTERIES ARE TRANSPORTED BY SHIP, VEHICLE AND RAILROAD
AVOID HIGH TEMPERATURE AND DEW CONDENSATION.

AVOID TRANSPORTATION WHICH MAY CAUSE DAMAGE OF PACKAGE.

LITHIUM-ION BATTERIES ARE NOT SUBJECT TO DANGEROUS GOODS REGULATION FOR THE
PURPOSE OF TRANSPORTATION BY THE INTERNATIONAL MARITIME DANGEROUS GOODS
REGULATIONS (IMDG). FOR LITHIUM-ION BATTERIES, THE WATT-HOUR RATING IS NO
MORE THAN 20WH /CELL AND 100WH/ BATTERY PACK CAN BE TREATED AS
"NON-DANGEROUS GOODS" BY THE UNITED NATIONS RECOMMENDATIONS ON THE
TRANSPORT OF DANGEROUS GOODS/SPECIAL PROVISION 188, PROVIDED THAT THE
PRODUCTS ARE PREVENTED FROM BEING SHORT-CIRCUITED WITH EACH OTHER AND ARE
PACKAGED IN AN APPROPRIATE CONDITION WHICH SATISFIES PACKING GROUP II
PERFORMANCE LEVEL.

IATA (INTERNATIONAL AIR TRANSPORT ASSOCIATION):
DANGEROUS GOODS REGULATION PACKING INSTRUCTION 965 (LITHIUM ION OR LITHIUM
POLYMER CELLS AND BATTERIES WITHOUT ELECTRONIC EQUIPMENT) WENT INTO EFFECT
APRIL 1, 2016: LITHIUM ION CELLS AND BATTERIES MUST BE OFFERED FOR
TRANSPORT AT A STATE OF CHARGE NOT EXCEEDING 30 PER CENT OF THEIR RATED
CAPACITY. UN 3480, PI 965, SECTION IA AND IB AND II WILL BE RESTRICTED TO
CARRIAGE ON CARGO AIRCRAFT. ALL PACKAGES MUST BEAR THE CARGO AIRCRAFT ONLY
LABEL IN ADDITION TO THE OTHER MARKS AND LABELS REQUIRED BY THE
REGULATIONS.

SECTION II REQUIREMENTS APPLY TO LITHIUM-ION CELLS WITH A WATT-HOUR RATING
NOT EXCEEDING 20 WH AND LITHIUM-ION BATTERIES WITH A WATT-HOUR RATING NOT
EXCEEDING 100 WH PACKED IN QUANTITIES THAT WITHIN THE ALLOWANCE PERMITTED
IN SECTION II, TABLE 965-11.

TABLE 965-II:

CONTENTS        LITHIUM-ION CELLS  LITHIUM-ION CELLS  LITHIUM-ION BATTERIES
                AND/OR BATTERIES   WITH A WATTHOUR    WITH A WATT-HOUR
                WITH A WATT-HOUR   RATING OF MORE     RATING OF MORE THAN
                RATING OF 2.7 WH   THAN 2.7WH BUT     2.7WH BUT NOT MORE
                OR LESS            NOT MORE THAN      THAN 100WH
                                   20WH

MAXIMUM NUMBER  NO LIMIT           8 CELLS            2 BATTERIES
OF CELLS /
BATTERIES PER
PACKAGE

MAXIMUM NET     2.5 KG             N/A                N/A
QUANTITY PER
PACKAGE

LITHIUM-ION CELLS AND BATTERIES MEETING THE REQUIREMENTS IN THIS SECTION
ARE NOT SUBJECT TO OTHER ADDITIONAL REQUIREMENTS OF THESE REGULATIONS
EXCEPT FOR:

EACH CELL AND BATTERY IS OF THE TYPE PROVEN TO MEET THE REQUIREMENTS OF
EACH TEST IN THE UN MANUAL OF TESTS AND CRITERIA, PART III, SUBSECTION
38.3;

CELLS AND BATTERIES MUST BE MANUFACTURED UNDER A QUALITY MANAGEMENT
PROGRAM;

FOR BATTERIES, THE WATT-HOUR RATING MUST BE MARKED ON THE OUTSIDE OF THE
BATTERY CASE;

EACH PACKAGE MUST BE CAPABLE OF WITHSTANDING A 1.2M DROP TEST IN ANY
ORIENTATION WITHOUT: DAMAGE TO CELLS OR BATTERIES CONTAINED THEREIN;
SHIFTING OF THE CONTENTS SO AS TO ALLOW BATTERY TO BATTERY (OR CELL TO
CELL) CONTACT; RELEASE OF CONTENTS.

EACH PACKAGE MUST BE LABELED WITH A LITHIUM BATTERY HANDLING LABEL.

SECTION IB REQUIREMENTS APPLY TO LITHIUM-ION CELLS WITH A WATT-HOUR RATING
NOT EXCEEDING 20 WH AND LITHIUM-ION BATTERIES WITH A WATT-HOUR RATING NOT
EXCEEDING 100 WH PACKED IN QUANTITIES THAT EXCEED THE ALLOWANCE PERMITTED
IN SECTION II, TABLE 965-II.

QUANTITIES OF LITHIUM-ION CELLS OR BATTERIES THAT EXCEED THE ALLOWANCE
PERMITTED IN SECTION II, TABLE 965-II MUST BE ASSIGNED TO CLASS 9 AND ARE
SUBJECT TO ALL OF THE APPLICABLE PROVISIONS OF REGULATION.

EVEN CLASSIFIED AS LITHIUM BATTERIES PACKED WITH EQUIPMENT (UN3481), IATA
DANGEROUS GOODS REGULATIONS PACKING INSTRUCTION 966 IS APPLIED.

EVEN CLASSIFIED AS LITHIUM BATTERIES INSTALLED IN EQUIPMENT (UN3481), IATA
DANGEROUS GOODS REGULATIONS PACKING INSTRUCTION 967 IS APPLIED.


SECTION 15. REGULATORY INFORMATION 


IMDG CODE: INTERNATIONAL MARITIME DANGEROUS GOODS (IMDG) CODE

ICAO TI:
INTERNATIONAL CIVIL AVIATION ORGANIZATION (ICAO) TECHNICAL INSTRUCTIONS FOR
THE SAFE TRANSPORT OF DANGEROUS GOODS BY AIR

IATA DGR:
INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) DANGEROUS GOODS REGULATIONS


SECTION 16. OTHER INFORMATION 


THE INFORMATION CONTAINED WITHIN IS PROVIDED FOR YOUR INFORMATION ONLY. THE
INFORMATION AND RECOMMENDATIONS SET FORTH HEREIN ARE MADE IN GOOD FAITH AND
ARE BELIEVED TO BE ACCURATE AS OF THE DATE OF PREPARATION. HOWEVER, MAKITA
U.S.A, INC. MAKES NO WARRANTY, EITHER EXPRESSED OR IMPLIED, WITH RESPECT
TO THIS INFORMATION AND DISCLAIMS ALL LIABILITY FROM RELIANCE ON IT.