Common Name: MOBILUX EP 0
Manufacturer: EXXON MOBIL
SDS Revision Date: 3/17/2015
SDS Format: GHS-US
   
Item Number(s): 53JW10
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 HAZARDS IDENTIFICATION 
SECTION 3 COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 4 FIRST AID MEASURES 
SECTION 5 FIRE FIGHTING MEASURES 
SECTION 6 ACCIDENTAL RELEASE MEASURES 
SECTION 7 HANDLING AND STORAGE 
SECTION 8 EXPOSURE CONTROLS / PERSONAL PROTECTION 
SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 STABILITY AND REACTIVITY 
SECTION 11 TOXICOLOGICAL INFORMATION 
SECTION 12 ECOLOGICAL INFORMATION 
SECTION 13 DISPOSAL CONSIDERATIONS 
SECTION 14 TRANSPORT INFORMATION 
SECTION 15 REGULATORY INFORMATION 
SECTION 16 OTHER INFORMATION 



EXXONMOBIL

PRODUCT NAME: MOBILUX EP 0

REVISION DATE: 17 MAR 2015

SAFETY DATA SHEET


SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT:

PRODUCT NAME: MOBILUX EP 0

PRODUCT DESCRIPTION: BASE OIL AND ADDITIVES

PRODUCT CODE: 2015A0208030, 641290-00, 971553

INTENDED USE: GREASE

COMPANY IDENTIFICATION:

SUPPLIER:
EXXON MOBIL CORPORATION
22777 SPRINGWOODS VILLAGE PARKWAY
SPRING, TX. 77389
USA

24 HOUR HEALTH EMERGENCY: 609-737-4411

TRANSPORTATION EMERGENCY PHONE: 800-424-9300 OR 703-527-3887 CHEMTREC

PRODUCT TECHNICAL INFORMATION: 800-662-4525

MSDS INTERNET ADDRESS:
HTTP://WWW.EXXON.COM
HTTP://WWW.MOBIL.COM


SECTION 2 HAZARDS IDENTIFICATION 


THIS MATERIAL IS NOT HAZARDOUS ACCORDING TO REGULATORY GUIDELINES (SEE
(M)SDS SECTION 15).

OTHER HAZARD INFORMATION:

HAZARD NOT OTHERWISE CLASSIFIED (HNOC):
NONE AS DEFINED UNDER 29 CFR 1910.1200.

PHYSICAL / CHEMICAL HAZARDS: NO SIGNIFICANT HAZARDS.

HEALTH HAZARDS:
HIGH-PRESSURE INJECTION UNDER SKIN MAY CAUSE SERIOUS DAMAGE. EXCESSIVE
EXPOSURE MAY RESULT IN EYE, SKIN, OR RESPIRATORY IRRITATION.

ENVIRONMENTAL HAZARDS: NO SIGNIFICANT HAZARDS.

NFPA HAZARD ID:
HEALTH       0
FLAMMABILITY 1
REACTIVITY   0

HMIS HAZARD ID:
HEALTH       0
FLAMMABILITY 1
REACTIVITY   0

NOTE:
THIS MATERIAL SHOULD NOT BE USED FOR ANY OTHER PURPOSE THAN THE INTENDED USE
IN SECTION 1 WITHOUT EXPERT ADVICE. HEALTH STUDIES HAVE SHOWN THAT CHEMICAL
EXPOSURE MAY CAUSE POTENTIAL HUMAN HEALTH RISKS WHICH MAY VARY FROM PERSON
TO PERSON.


SECTION 3 COMPOSITION / INFORMATION ON INGREDIENTS 


THIS MATERIAL IS DEFINED AS A MIXTURE.

HAZARDOUS SUBSTANCE(S) OR COMPLEX SUBSTANCE(S) REQUIRED FOR DISCLOSURE:

NAME                  CAS#         CONCENTRATION*    GHS HAZARD CODES

PHOSPHORIC ACID       61188-14-5   0.1-<1%           H318, H401, H411
ESTERS, AMINE SALT

ZINC DITHIOPHOSPHATE  68649-42-3     1-2.5%          H315, H318, H401, H411

* ALL CONCENTRATIONS ARE PERCENT BY WEIGHT UNLESS MATERIAL IS A GAS. GAS
CONCENTRATIONS ARE IN PERCENT BY VOLUME.

AS PER PARAGRAPH (I) OF 29 CFR 1910.1200, FORMULATION IS CONSIDERED A TRADE
SECRET AND SPECIFIC CHEMICAL IDENTITY AND EXACT PERCENTAGE (CONCENTRATION)
OF COMPOSITION MAY HAVE BEEN WITHHELD. SPECIFIC CHEMICAL IDENTITY AND EXACT
PERCENTAGE COMPOSITION WILL BE PROVIDED TO HEALTH PROFESSIONALS, EMPLOYEES,
OR DESIGNATED REPRESENTATIVES IN ACCORDANCE WITH APPLICABLE PROVISIONS OF
PARAGRAPH (I).


SECTION 4 FIRST AID MEASURES 


INHALATION:
UNDER NORMAL CONDITIONS OF INTENDED USE, THIS MATERIAL IS NOT EXPECTED TO BE
AN INHALATION HAZARD.

SKIN CONTACT:
WASH CONTACT AREAS WITH SOAP AND WATER. IF PRODUCT IS INJECTED INTO OR UNDER
THE SKIN, OR INTO ANY PART OF THE BODY, REGARDLESS OF THE APPEARANCE OF THE
WOUND OR ITS SIZE, THE INDIVIDUAL SHOULD BE EVALUATED IMMEDIATELY BY A
PHYSICIAN AS A SURGICAL EMERGENCY. EVEN THOUGH INITIAL SYMPTOMS FROM HIGH
PRESSURE INJECTION MAY BE MINIMAL OR ABSENT, EARLY SURGICAL TREATMENT WITHIN
THE FIRST FEW HOURS MAY SIGNIFICANTLY REDUCE THE ULTIMATE EXTENT OF INJURY.

EYE CONTACT:
FLUSH THOROUGHLY WITH WATER. IF IRRITATION OCCURS, GET MEDICAL ASSISTANCE.

INGESTION:
FIRST AID IS NORMALLY NOT REQUIRED. SEEK MEDICAL ATTENTION IF DISCOMFORT
OCCURS.


SECTION 5 FIRE FIGHTING MEASURES 


EXTINGUISHING MEDIA:

APPROPRIATE EXTINGUISHING MEDIA:
USE WATER FOG, FOAM, DRY CHEMICAL OR CARBON DIOXIDE (CO2) TO EXTINGUISH
FLAMES.

INAPPROPRIATE EXTINGUISHING MEDIA: STRAIGHT STREAMS OF WATER

FIRE FIGHTING:

FIRE FIGHTING INSTRUCTIONS:
EVACUATE AREA. PREVENT RUNOFF FROM FIRE CONTROL OR DILUTION FROM ENTERING
STREAMS, SEWERS, OR DRINKING WATER SUPPLY. FIREFIGHTERS SHOULD USE STANDARD
PROTECTIVE EQUIPMENT AND IN ENCLOSED SPACES, SELF-CONTAINED BREATHING
APPARATUS (SCBA). USE WATER SPRAY TO COOL FIRE EXPOSED SURFACES AND TO
PROTECT PERSONNEL.

HAZARDOUS COMBUSTION PRODUCTS:
SULFUR OXIDES, INCOMPLETE COMBUSTION PRODUCTS, ALDEHYDES, OXIDES OF CARBON,
SMOKE, FUME

FLAMMABILITY PROPERTIES:

FLASH POINT [METHOD]:
>204 DEG. C (400 DEG. F) [EST. FOR OIL, ASTM D-92 (COC)]

FLAMMABLE LIMITS (APPROXIMATE VOLUME % IN AIR):
LEL: N/D
UEL: N/D

AUTOIGNITION TEMPERATURE: N/D


SECTION 6 ACCIDENTAL RELEASE MEASURES 


NOTIFICATION PROCEDURES:
IN THE EVENT OF A SPILL OR ACCIDENTAL RELEASE, NOTIFY RELEVANT AUTHORITIES
IN ACCORDANCE WITH ALL APPLICABLE REGULATIONS. US REGULATIONS REQUIRE
REPORTING RELEASES OF THIS MATERIAL TO THE ENVIRONMENT WHICH EXCEED THE
APPLICABLE REPORTABLE QUANTITY OR OIL SPILLS WHICH COULD REACH ANY WATERWAY
INCLUDING INTERMITTENT DRY CREEKS. THE NATIONAL RESPONSE CENTER CAN BE
REACHED AT (800)424-8802.

PROTECTIVE MEASURES:
AVOID CONTACT WITH SPILLED MATERIAL. SEE SECTION 5 FOR FIRE FIGHTING
INFORMATION. SEE THE HAZARD IDENTIFICATION SECTION FOR SIGNIFICANT HAZARDS.
SEE SECTION 4 FOR FIRST AID ADVICE. SEE SECTION 8 FOR ADVICE ON THE MINIMUM
REQUIREMENTS FOR PERSONAL PROTECTIVE EQUIPMENT. ADDITIONAL PROTECTIVE
MEASURES MAY BE NECESSARY, DEPENDING ON THE SPECIFIC CIRCUMSTANCES AND/OR
THE EXPERT JUDGMENT OF THE EMERGENCY RESPONDERS.

FOR EMERGENCY RESPONDERS:
RESPIRATORY PROTECTION:
RESPIRATORY PROTECTION WILL BE NECESSARY ONLY IN SPECIAL CASES, E.G.,
FORMATION OF MISTS. HALF-FACE OR FULL-FACE RESPIRATOR WITH FILTER(S) FOR
DUST/ORGANIC VAPOR OR SELF CONTAINED BREATHING APPARATUS (SCBA) CAN BE USED
DEPENDING ON THE SIZE OF SPILL AND POTENTIAL LEVEL OF EXPOSURE. IF THE
EXPOSURE CANNOT BE COMPLETELY CHARACTERIZED OR AN OXYGEN DEFICIENT
ATMOSPHERE IS POSSIBLE OR ANTICIPATED, SCBA IS RECOMMENDED. WORK GLOVES THAT
ARE RESISTANT TO HYDROCARBONS ARE RECOMMENDED. GLOVES MADE OF POLYVINYL
ACETATE (PVA) ARE NOT WATER-RESISTANT AND ARE NOT SUITABLE FOR EMERGENCY
USE. CHEMICAL GOGGLES ARE RECOMMENDED IF SPLASHES OR CONTACT WITH EYES IS
POSSIBLE.

SMALL SPILLS: NORMAL ANTISTATIC WORK CLOTHES ARE USUALLY ADEQUATE.

LARGE SPILLS:
FULL BODY SUIT OF CHEMICAL RESISTANT, ANTISTATIC MATERIAL IS RECOMMENDED.

SPILL MANAGEMENT:

LAND SPILL:
ALLOW SPILLED MATERIAL TO SOLIDIFY AND SCRAPE UP WITH SHOVELS INTO A
SUITABLE CONTAINER FOR RECYCLE OR DISPOSAL. SCRAPE UP SPILLED MATERIAL
WITH SHOVELS INTO A SUITABLE CONTAINER FOR RECYCLE OR DISPOSAL.

WATER SPILL:
STOP LEAK IF YOU CAN DO IT WITHOUT RISK. CONFINE THE SPILL IMMEDIATELY
WITH BOOMS. WARN OTHER SHIPPING. SKIM FROM SURFACE.

WATER SPILL AND LAND SPILL RECOMMENDATIONS ARE BASED ON THE MOST LIKELY
SPILL SCENARIO FOR THIS MATERIAL; HOWEVER, GEOGRAPHIC CONDITIONS, WIND,
TEMPERATURE, (AND IN THE CASE OF A WATER SPILL) WAVE AND CURRENT DIRECTION
AND SPEED MAY GREATLY INFLUENCE THE APPROPRIATE ACTION TO BE TAKEN. FOR THIS
REASON, LOCAL EXPERTS SHOULD BE CONSULTED.

NOTE: LOCAL REGULATIONS MAY PRESCRIBE OR LIMIT ACTION TO BE TAKEN.

ENVIRONMENTAL PRECAUTIONS:
PREVENT ENTRY INTO WATERWAYS, SEWERS, BASEMENTS OR CONFINED AREAS.


SECTION 7 HANDLING AND STORAGE 


HANDLING: PREVENT SMALL SPILLS AND LEAKAGE TO AVOID SLIP HAZARD.

STATIC ACCUMULATOR: THIS MATERIAL IS NOT A STATIC ACCUMULATOR.

STORAGE: DO NOT STORE IN OPEN OR UNLABELLED CONTAINERS.


SECTION 8 EXPOSURE CONTROLS / PERSONAL PROTECTION 


NOTE:
LIMITS/STANDARDS SHOWN FOR GUIDANCE ONLY. FOLLOW APPLICABLE REGULATIONS.
NO BIOLOGICAL LIMITS ALLOCATED.

ENGINEERING CONTROLS:
THE LEVEL OF PROTECTION AND TYPES OF CONTROLS NECESSARY WILL VARY DEPENDING
UPON POTENTIAL EXPOSURE CONDITIONS.

CONTROL MEASURES TO CONSIDER:
NO SPECIAL REQUIREMENTS UNDER ORDINARY CONDITIONS OF USE AND WITH ADEQUATE
VENTILATION.

PERSONAL PROTECTION:
PERSONAL PROTECTIVE EQUIPMENT SELECTIONS VARY BASED ON POTENTIAL EXPOSURE
CONDITIONS SUCH AS APPLICATIONS, HANDLING PRACTICES, CONCENTRATION AND
VENTILATION. INFORMATION ON THE SELECTION OF PROTECTIVE EQUIPMENT FOR USE
WITH THIS MATERIAL, AS PROVIDED BELOW, IS BASED UPON INTENDED, NORMAL USAGE.

RESPIRATORY PROTECTION:
IF ENGINEERING CONTROLS DO NOT MAINTAIN AIRBORNE CONTAMINANT CONCENTRATIONS
AT A LEVEL WHICH IS ADEQUATE TO PROTECT WORKER HEALTH, AN APPROVED
RESPIRATOR MAY BE APPROPRIATE. RESPIRATOR SELECTION, USE, AND MAINTENANCE
MUST BE IN ACCORDANCE WITH REGULATORY REQUIREMENTS, IF APPLICABLE.

TYPES OF RESPIRATORS TO BE CONSIDERED FOR THIS MATERIAL INCLUDE:
NO PROTECTION IS ORDINARILY REQUIRED UNDER NORMAL CONDITIONS OF USE AND
WITH ADEQUATE VENTILATION.

FOR HIGH AIRBORNE CONCENTRATIONS, USE AN APPROVED SUPPLIED-AIR RESPIRATOR,
OPERATED IN POSITIVE PRESSURE MODE. SUPPLIED AIR RESPIRATORS WITH AN ESCAPE
BOTTLE MAY BE APPROPRIATE WHEN OXYGEN LEVELS ARE INADEQUATE, GAS/VAPOR
WARNING PROPERTIES ARE POOR, OR IF AIR PURIFYING FILTER CAPACITY/RATING MAY
BE EXCEEDED.

HAND PROTECTION:
ANY SPECIFIC GLOVE INFORMATION PROVIDED IS BASED ON PUBLISHED LITERATURE AND
GLOVE MANUFACTURER DATA. GLOVE SUITABILITY AND BREAKTHROUGH TIME WILL DIFFER
DEPENDING ON THE SPECIFIC USE CONDITIONS. CONTACT THE GLOVE MANUFACTURER FOR
SPECIFIC ADVICE ON GLOVE SELECTION AND BREAKTHROUGH TIMES FOR YOUR USE
CONDITIONS. INSPECT AND REPLACE WORN OR DAMAGED GLOVES.

THE TYPES OF GLOVES TO BE CONSIDERED FOR THIS MATERIAL INCLUDE:
NO PROTECTION IS ORDINARILY REQUIRED UNDER NORMAL CONDITIONS OF USE.

EYE PROTECTION:
IF CONTACT IS LIKELY, SAFETY GLASSES WITH SIDE SHIELDS ARE RECOMMENDED.

SKIN AND BODY PROTECTION:
ANY SPECIFIC CLOTHING INFORMATION PROVIDED IS BASED ON PUBLISHED LITERATURE
OR MANUFACTURER DATA.

THE TYPES OF CLOTHING TO BE CONSIDERED FOR THIS MATERIAL INCLUDE:
NO SKIN PROTECTION IS ORDINARILY REQUIRED UNDER NORMAL CONDITIONS OF USE.
IN ACCORDANCE WITH GOOD INDUSTRIAL HYGIENE PRACTICES, PRECAUTIONS SHOULD
BE TAKEN TO AVOID SKIN CONTACT.

SPECIFIC HYGIENE MEASURES:
ALWAYS OBSERVE GOOD PERSONAL HYGIENE MEASURES, SUCH AS WASHING AFTER
HANDLING THE MATERIAL AND BEFORE EATING, DRINKING, AND/OR SMOKING.
ROUTINELY WASH WORK CLOTHING AND PROTECTIVE EQUIPMENT TO REMOVE
CONTAMINANTS. DISCARD CONTAMINATED CLOTHING AND FOOTWEAR THAT CANNOT BE
CLEANED. PRACTICE GOOD HOUSEKEEPING.

ENVIRONMENTAL CONTROLS:
COMPLY WITH APPLICABLE ENVIRONMENTAL REGULATIONS LIMITING DISCHARGE TO AIR,
WATER AND SOIL. PROTECT THE ENVIRONMENT BY APPLYING APPROPRIATE CONTROL
MEASURES TO PREVENT OR LIMIT EMISSIONS.


SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 


NOTE:
PHYSICAL AND CHEMICAL PROPERTIES ARE PROVIDED FOR SAFETY, HEALTH AND
ENVIRONMENTAL CONSIDERATIONS ONLY AND MAY NOT FULLY REPRESENT PRODUCT
SPECIFICATIONS. CONTACT THE SUPPLIER FOR ADDITIONAL INFORMATION.

GENERAL INFORMATION:
PHYSICAL STATE: SOLID

FORM: SEMI-FLUID

COLOR: BROWN

ODOR: CHARACTERISTIC

ODOR THRESHOLD: N/D

IMPORTANT HEALTH, SAFETY, AND ENVIRONMENTAL INFORMATION:

RELATIVE DENSITY (AT 15 DEG. C): 0.918

FLAMMABILITY (SOLID, GAS):

FLASH POINT [METHOD]:
>204 DEG. C (400 DEG. F) [EST. FOR OIL, ASTM D-92 (COC)]

FLAMMABLE LIMITS (APPROXIMATE VOLUME % IN AIR):
LEL: N/D
UEL: N/D

AUTOIGNITION TEMPERATURE: N/D

BOILING POINT / RANGE: >316 DEG. C (600 DEG. F)

DECOMPOSITION TEMPERATURE: N/D

VAPOR DENSITY (AIR = 1): N/D

VAPOR PRESSURE: <0.013 KPA(0.1 MMHg) AT 20 DEG. C

EVAPORATION RATE (N-BUTYL ACETATE = 1): N/D

PH: N/A

LOG POW (N-OCTANOL/WATER PARTITION COEFFICIENT): >3.5

SOLUBILITY IN WATER: NEGLIGIBLE

VISCOSITY: 150 CST (150 MM2/SEC) AT 40 DEG. C

OXIDIZING PROPERTIES: SEE HAZARDS IDENTIFICATION SECTION.

OTHER INFORMATION:
FREEZING POINT: N/D
MELTING POINT: N/D
DMSO EXTRACT (MINERAL OIL ONLY), IP-346: <3%WT

NOTE:
MOST PHYSICAL PROPERTIES ABOVE ARE FOR THE OIL COMPONENT IN THE MATERIAL.


SECTION 10 STABILITY AND REACTIVITY 


REACTIVITY: SEE SUB-SECTIONS BELOW.

STABILITY: MATERIAL IS STABLE UNDER NORMAL CONDITIONS.

CONDITIONS TO AVOID: EXCESSIVE HEAT. HIGH ENERGY SOURCES OF IGNITION.

MATERIALS TO AVOID: STRONG OXIDIZERS

HAZARDOUS DECOMPOSITION PRODUCTS:
MATERIAL DOES NOT DECOMPOSE AT AMBIENT TEMPERATURES.

POSSIBILITY OF HAZARDOUS REACTIONS: HAZARDOUS POLYMERIZATION WILL NOT OCCUR.


SECTION 11 TOXICOLOGICAL INFORMATION 


INFORMATION ON TOXICOLOGICAL EFFECTS:

HAZARD CLASS                     CONCLUSION / REMARKS

INHALATION:
ACUTE TOXICITY:                  MINIMALLY TOXIC. BASED ON ASSESSMENT OF THE
NO END POINT DATA FOR MATERIAL.  COMPONENTS.

IRRITATION:                      NEGLIGIBLE HAZARD AT AMBIENT/NORMAL
NO END POINT DATA FOR MATERIAL.  HANDLING TEMPERATURES.

INGESTION:
ACUTE TOXICITY:                  MINIMALLY TOXIC. BASED ON ASSESSMENT OF THE
NO END POINT DATA FOR MATERIAL.  COMPONENTS.

SKIN:
ACUTE TOXICITY:                  MINIMALLY TOXIC. BASED ON ASSESSMENT OF THE
NO END POINT DATA FOR MATERIAL.  COMPONENTS.

SKIN CORROSION/IRRITATION:       NEGLIGIBLE IRRITATION TO SKIN AT AMBIENT
NO END POINT DATA FOR MATERIAL.  TEMPERATURES. BASED ON ASSESSMENT OF THE
                                 COMPONENTS.

EYE:
SERIOUS EYE DAMAGE/IRRITATION:   MAY CAUSE MILD, SHORT-LASTING DISCOMFORT TO
NO END POINT FOR MATERIAL.       EYES. BASED ON DATA  ASSESSMENT OF THE
                                 COMPONENTS.

SENSITIZATION:

RESPIRATORY SENSITIZATION:       NOT EXPECTED TO BE A RESPIRATORY
NO END POINT DATA FOR MATERIAL.  SENSITIZER.

SKIN SENSITIZATION:              NOT EXPECTED TO BE A SKIN SENSITIZER. BASED
NO END POINT DATA FOR MATERIAL.  ON ASSESSMENT OF THE COMPONENTS.

ASPIRATION: DATA AVAILABLE.      NOT EXPECTED TO BE AN ASPIRATION HAZARD.
                                 BASED ON PHYSICO-CHEMICAL PROPERTIES OF THE
                                 MATERIAL.

GERM CELL MUTAGENICITY:          NOT EXPECTED TO BE A GERM CELL MUTAGEN.
NO END POINT DATA FOR MATERIAL.  BASED ON ASSESSMENT OF THE COMPONENTS.

CARCINOGENICITY:                 NOT EXPECTED TO CAUSE CANCER. BASED ON
NO END POINT DATA FOR MATERIAL.  ASSESSMENT OF THE COMPONENTS.

REPRODUCTIVE TOXICITY:           NOT EXPECTED TO BE A REPRODUCTIVE TOXICANT.
NO END POINT DATA FOR MATERIAL.  BASED ON ASSESSMENT OF THE COMPONENTS.

LACTATION:                       NOT EXPECTED TO CAUSE HARM TO BREAST-FED
NO END POINT DATA FOR MATERIAL.  CHILDREN.

SPECIFIC TARGET ORGAN TOXICITY (STOT):

SINGLE EXPOSURE:                 NOT EXPECTED TO CAUSE ORGAN DAMAGE FROM A
NO END POINT DATA FOR MATERIAL.  SINGLE EXPOSURE.

REPEATED EXPOSURE:               NOT EXPECTED TO CAUSE ORGAN DAMAGE FROM
NO END POINT DATA FOR MATERIAL.  PROLONGED OR REPEATED EXPOSURE. BASED ON
                                 ASSESSMENT OF THE COMPONENTS.

OTHER INFORMATION:

CONTAINS:

BASE OIL SEVERELY REFINED:
NOT CARCINOGENIC IN ANIMAL STUDIES. REPRESENTATIVE MATERIAL PASSES IP-346,
MODIFIED AMES TEST, AND/OR OTHER SCREENING TESTS. DERMAL AND INHALATION
STUDIES SHOWED MINIMAL EFFECTS; LUNG NON-SPECIFIC INFILTRATION OF IMMUNE
CELLS, OIL DEPOSITION AND MINIMAL GRANULOMA FORMATION. NOT SENSITIZING IN
TEST ANIMALS.

THE FOLLOWING INGREDIENTS ARE CITED ON THE LISTS BELOW: NONE.

REGULATORY LISTS SEARCHED:
1 = NTP CARC
2 = NTP SUS
3 = IARC 1
4 = IARC 2A
5 = IARC 2B
6 = OSHA CARC


SECTION 12 ECOLOGICAL INFORMATION 


THE INFORMATION GIVEN IS BASED ON DATA AVAILABLE FOR THE MATERIAL, THE
COMPONENTS OF THE MATERIAL, AND SIMILAR MATERIALS.

ECOTOXICITY:
MATERIAL: NOT EXPECTED TO BE HARMFUL TO AQUATIC ORGANISMS.

MOBILITY:
BASE OIL COMPONENT:
LOW SOLUBILITY AND FLOATS AND IS EXPECTED TO MIGRATE FROM WATER TO THE LAND.
EXPECTED TO PARTITION TO SEDIMENT AND WASTEWATER SOLIDS.

PERSISTENCE AND DEGRADABILITY:

BIODEGRADATION:
BASE OIL COMPONENT: EXPECTED TO BE INHERENTLY BIODEGRADABLE

BIOACCUMULATION POTENTIAL:
BASE OIL COMPONENT:
HAS THE POTENTIAL TO BIOACCUMULATE, HOWEVER METABOLISM OR PHYSICAL
PROPERTIES MAY REDUCE THE BIOCONCENTRATION OR LIMIT BIOAVAILABILITY.


SECTION 13 DISPOSAL CONSIDERATIONS 


DISPOSAL RECOMMENDATIONS BASED ON MATERIAL AS SUPPLIED. DISPOSAL MUST BE
IN ACCORDANCE WITH CURRENT APPLICABLE LAWS AND REGULATIONS, AND MATERIAL
CHARACTERISTICS AT TIME OF DISPOSAL.

DISPOSAL RECOMMENDATIONS:
PRODUCT IS SUITABLE FOR BURNING IN AN ENCLOSED CONTROLLED BURNER FOR FUEL
VALUE OR DISPOSAL BY SUPERVISED INCINERATION AT VERY HIGH TEMPERATURES TO
PREVENT FORMATION OF UNDESIRABLE COMBUSTION PRODUCTS.

REGULATORY DISPOSAL INFORMATION:

RCRA INFORMATION:
THE UNUSED PRODUCT, IN OUR OPINION, IS NOT SPECIFICALLY LISTED BY THE EPA AS
A HAZARDOUS WASTE (40 CFR, PART 261D), NOR IS IT FORMULATED TO CONTAIN
MATERIALS WHICH ARE LISTED AS HAZARDOUS WASTES. IT DOES NOT EXHIBIT THE
HAZARDOUS CHARACTERISTICS OF IGNITABILITY, CORROSITIVITY OR REACTIVITY AND
IS NOT FORMULATED WITH CONTAMINANTS AS DETERMINED BY THE TOXICITY
CHARACTERISTIC LEACHING PROCEDURE (TCLP). HOWEVER, USED PRODUCT MAY BE
REGULATED.

EMPTY CONTAINER WARNING EMPTY CONTAINER WARNING (WHERE APPLICABLE):
EMPTY CONTAINERS MAY CONTAIN RESIDUE AND CAN BE DANGEROUS. DO NOT ATTEMPT TO
REFILL OR CLEAN CONTAINERS WITHOUT PROPER INSTRUCTIONS. EMPTY DRUMS SHOULD
BE COMPLETELY DRAINED AND SAFELY STORED UNTIL APPROPRIATELY RECONDITIONED OR
DISPOSED. EMPTY CONTAINERS SHOULD BE TAKEN FOR RECYCLING, RECOVERY, OR
DISPOSAL THROUGH SUITABLY QUALIFIED OR LICENSED CONTRACTOR AND IN ACCORDANCE
WITH GOVERNMENTAL REGULATIONS. DO NOT PRESSURISE, CUT, WELD, BRAZE, SOLDER,
DRILL, GRIND, OR EXPOSE SUCH CONTAINERS TO HEAT, FLAME, SPARKS, STATIC
ELECTRICITY, OR OTHER SOURCES OF IGNITION. THEY MAY EXPLODE AND CAUSE INJURY
OR DEATH.


SECTION 14 TRANSPORT INFORMATION 


LAND (DOT): NOT REGULATED FOR LAND TRANSPORT

LAND (TDG): NOT REGULATED FOR LAND TRANSPORT

SEA (IMDG): NOT REGULATED FOR SEA TRANSPORT ACCORDING TO IMDG-CODE

MARINE POLLUTANT: NO

AIR (IATA): NOT REGULATED FOR AIR TRANSPORT


SECTION 15 REGULATORY INFORMATION 


OSHA HAZARD COMMUNICATION STANDARD:
THIS MATERIAL IS NOT CONSIDERED HAZARDOUS IN ACCORDANCE WITH OSHA HAZCOM
2012, 29 CFR 1910.1200.

LISTED OR EXEMPT FROM LISTING/NOTIFICATION ON THE FOLLOWING CHEMICAL
INVENTORIES: DSL, KECI, PICCS, TSCA

SPECIAL CASES:

INVENTORY           STATUS

AICS                RESTRICTIONS APPLY

EPCRA SECTION 302: THIS MATERIAL CONTAINS NO EXTREMELY HAZARDOUS SUBSTANCES.

SARA (311/312) REPORTABLE HAZARD CATEGORIES: NONE.

SARA (313) TOXIC RELEASE INVENTORY:

CHEMICAL NAME              CAS NUMBER        TYPICAL VALUE

ZINC DITHIOPHOSPHATE       68649-42-3        1 - 2.5%

THE FOLLOWING INGREDIENTS ARE CITED ON THE LISTS BELOW:

CHEMICAL NAME              CAS NUMBER        LIST CITATIONS

DIPHENYLAMINE                122-39-4        18

ZINC DITHIOPHOSPHATE       68649-42-3        13, 15, 17, 19

REGULATORY LISTS SEARCHED:
1 = ACGIH ALL
2 = ACGIH A1
3 = ACGIH A2
4 = OSHA Z
5 = TSCA 4
6 = TSCA 5A2
7 = TSCA 5E
8 = TSCA 6
9 = TSCA 12B
10 = CA P65 CARC
11 = CA P65 REPRO
12 = CA RTK
13 = IL RTK
14 = LA RTK
15 = MI 293
16 = MN RTK
17 = NJ RTK
18 = PA RTK
19 = RI RTK

CODE KEY:
CARC=CARCINOGEN
REPRO=REPRODUCTIVE


SECTION 16 OTHER INFORMATION 


N/D = NOT DETERMINED
N/A = NOT APPLICABLE

KEY TO THE H-CODES CONTAINED IN SECTION 3 OF THIS DOCUMENT (FOR INFORMATION
ONLY):
H315: CAUSES SKIN IRRITATION; SKIN CORR/IRRITATION, CAT 2

H318: CAUSES SERIOUS EYE DAMAGE; SERIOUS EYE DAMAGE/IRR, CAT 1

H401: TOXIC TO AQUATIC LIFE; ACUTE ENV TOX, CAT 2

H411:
TOXIC TO AQUATIC LIFE WITH LONG LASTING EFFECTS; CHRONIC ENV TOX, CAT 2

THIS SAFETY DATA SHEET CONTAINS THE FOLLOWING REVISIONS:
UPDATES MADE IN ACCORDANCE WITH IMPLEMENTATION OF GHS REQUIREMENTS.

THE INFORMATION AND RECOMMENDATIONS CONTAINED HEREIN ARE, TO THE BEST OF
EXXONMOBIL'S KNOWLEDGE AND BELIEF, ACCURATE AND RELIABLE AS OF THE DATE
ISSUED. YOU CAN CONTACT EXXONMOBIL TO INSURE THAT THIS DOCUMENT IS THE MOST
CURRENT AVAILABLE FROM EXXONMOBIL. THE INFORMATION AND RECOMMENDATIONS ARE
OFFERED FOR THE USER'S CONSIDERATION AND EXAMINATION. IT IS THE USER'S
RESPONSIBILITY TO SATISFY ITSELF THAT THE PRODUCT IS SUITABLE FOR THE
INTENDED USE. IF BUYER REPACKAGES THIS PRODUCT, IT IS THE USER'S
RESPONSIBILITY TO INSURE PROPER HEALTH, SAFETY AND OTHER NECESSARY
INFORMATION IS INCLUDED WITH AND/OR ON THE CONTAINER. APPROPRIATE WARNINGS
AND SAFE-HANDLING PROCEDURES SHOULD BE PROVIDED TO HANDLERS AND USERS.
ALTERATION OF THIS DOCUMENT IS STRICTLY PROHIBITED. EXCEPT TO THE EXTENT
REQUIRED BY LAW, RE-PUBLICATION OR RETRANSMISSION OF THIS DOCUMENT, IN
WHOLE OR IN PART, IS NOT PERMITTED. THE TERM, "EXXONMOBIL" IS USED FOR
CONVENIENCE, AND MAY INCLUDE ANY ONE OR MORE OF EXXONMOBIL CHEMICAL COMPANY,
EXXON MOBIL CORPORATION, OR ANY AFFILIATES IN WHICH THEY DIRECTLY OR
INDIRECTLY HOLD ANY INTEREST.

INTERNAL USE ONLY:
MHC: OB, OB, 0, 0, 0, 0
PPEC: A

DGN: 2009904XUS (553448)

COPYRIGHT 2002 EXXON MOBIL CORPORATION, ALL RIGHTS RESERVED